Hi all,
i have a problem running any tools from the RTOS or System Analyzer. I just wanted to see the logs i create using log_entry{n}() while debugging my program.
When i want to start one of those tools (eg. RTOS Analyzer > Printf and Error Logs), i get the error message in the popup window (see screenshot1), saying:
Could not detect a UIA configuration. One of the following is required:
* Either load a program with UIA instrumentation turned on
* Or specify a custom UIA configuration
I use the following components:
- CCS 6.1.0.00104
- SYS/BIOS 6.41.3.51
- XDCtools 3.30.6.67_core
- UIA 2.0.2.39
- MCSDK 2.1.2.6
- IPC 3.30.1.12
- EDMA3 Low Level Driver 2.12.0
- Device: TMS320C6678
- Debug Probe: BlackHawk XDS560v2 (USB)
- Windows 7 SP1
Please help me to get this stuff running! Thanks in advance,
Greets Stefan