Thanks in advance for the help !!
I have 2 questions:
1) All of the code I am migrating include the file XXXcfg.h because is (used to) contain the declarations of all the specific Project objects created from the XXX.tcf file (SEM_foo1, LCK_foo2, etc). Now that I have converted my TCF file to a CFG file and created a platform, those declarations are gone. Yes, the new XXXcfg.h file does #include <xdc/cfg/global.h> but that only gives me the declarations for the BIOS Object Types and functions. Did I miss something in the conversion ? What is supposed to take the place of the original XXXcfg.h, that contains declarations for the PROJECT defined Objects ??
2) When running the XGCONF tool on my new XXX.cfg file (project test1) I get this error:
Description Resource Path Location Type
java.lang.ArrayIndexOutOfBoundsException: 6 SYS1.cfg /test1 Configuration Validation XDCTools Configuration Marker
and if I try to build the new XXX.cfg file I get this additional error:
Description Resource Path Location Type
gmake: *** No rule to make target `SYS1.opt'. Stop. test1 Unknown C/C++ Problem
Can you help me track this issue down ? The error messages are not very specific !!