I am building a DSP/BIOS project using SYS/BIOS (CCSv5). I have conquered the configuration conversions and seem to be compiling the source code just fine. The original project has a boot file in it that looks to be copies of some of the initial startup functions - taken directly from DSP/BIOS source code. Now, when I link, I get:
error #10056: symbol "_c_int00" redefined: first defined in "./boot.obj"; redefined in "C:\ti\bios_6_35_04_50\packages\ti\bios\support\lib\release\ti.bios.support.a64P<boot.o64P>"
error #10056: symbol "__stack" redefined: first defined in "./boot.obj"; redefined in "C:\ti\bios_6_35_04_50\packages\ti\bios\support\lib\release\ti.bios.support.a64P<boot.o64P>"
error #10056: symbol "__auto_init" redefined: first defined in "./autoinit.obj"; redefined in "C:\ti\xdctools_3_23_04_60\packages\ti\targets\rts6000\lib\boot.a64P<autoinit.o64P>"
warning #10247-D: creating output section ".bios" without a SECTIONS specification
How can I change the settings for the linker phase such that it doesn't pull-in the SYS/BIOS versions of those functions ?
Thanks !!