Hi,
I am using TM4C1294NCPDT on EK-1294XL board. tirtos_tivac_2_14_04_3, TivaWare_C_Series-2.1.2.111, CCS_6.1.2.00015 versions on Windows 8 64-bit machine.
I have taken HTTP GET example code from TI-RTOS and trying to use simple socket code for GET and POST Request. Issue is whenever it tries to create socket using either socket() or NDK_socket() method it is going into Hardware exception (ti_sysbios_family_arm_m3_Hwi_excHandlerAsm__I). Why it is not allowing to create socket?
Attached is the code.
Thanks,
Bhavesh