Hi,
We have issue with the NDK TCP/IP communication on TM4C129xx.
The network doesn't work properly during re-connection.
Currently one of our customer is trying to build a server application
with TM4C129xx, where a task is executed inside Network open hook function
and the settings of IPAddress, Subnet, gateway etc are done in CfgAddEntry()
and re-connection is executed immediately if there is a disconnection with the Client, .
・Device used :TM4C1294NCPDTI
・IDE :CCS v6.0.0
・OS :TI-RTOS 2.01.00.03
:bios_6_40_03_39
:ndk_2_23_01_01
Problem:
After the disconnection from the client,we are not able to re-connect.
Failure Procedure.
1.After connecting server to the client, disconnect from the Client
2.Close the Client Socket and Server socket with fdclose() and
again create the Server socket with socket() function.
3.It fails in bind() and the fdError() is 「48」
Please let us know if there is any way to solve this issue.
Best Regards