Dear all,
I am experiencing a few oddities with the RTC clock and CCS as well.
I need to use the RTC clock to know the local time after an hibernation, thus i used a template project to experience it first hand. The RTC works flawlessly so far. I can set the time, and get the increased value after the hibernation ends.
Then I include the same procedure in my working project, but every time the CC3200 wake up the RTC clock returns a number that actually matches the number of hybernation cycles with a minus sign on top of it (is that even a feature of some sort ??).
At this point I start stripping the code from the working project, to remove every feature that may cause a conflict. The issue remains.
After stripping the code, the working project is almost identical to the template project. The only difference is the "File search path" in the preferences.
Since the issue is still there, I remove a few entries from the path. The problem is apparently solved but when I put back the same entries, the issue does not show up. What is the meaning of that? If the libraries are not causing a conflict, why the issue kept popping out before I removed them?
If the cause is elsewhere, why did it keep popping out even though I removed the cause, and stopped only after I removed the path from the properties?
Is there some kind of cache in CCS?
And most of all why the hell the RTC keeps stop counting??
Thank you for your kind answers beforehand.