Hello,
HW: TM4C129EXL-LP | RTOS : 2.14.4.31 |
I have faced the following issue:
ss in flash Starting the TCP Echo example System provider is set to SysMin. Halt the target to view any SysMin contents in ROV. Service Status: DHCPC : Enabled : : 000 Network Open Hook Fired Service Status: DHCPC : Enabled : Running : 000 Network Added: If-1:192.168.3.2 Network IP Address Hook Fired Service Status: DHCPC : Enabled : Running : 017 00012.200 TcpTimeoutRexmt: Retransmit Timeout Network Removed: If-1:192.168.3.2 Network IP Address Hook Fired Service Status: DHCPC : Disabled : : 000 Network Close Hook Fired FSR = 0x0000 HFSR = 0x40000000 DFSR = 0x0000000b MMAR = 0xe000ed34 BFAR = 0xe000ed38 AFSR = 0x00000000 Terminating execution...
The target is configured to obtain IP address automatically from the router. On the router side I modified Default Subnet Mask from 255.255.255.0 to 255.255.255.240 and set the new IP range as you can see on the attached picture.
When I tried to connect with this new router config I can not connect to target and gave me the error aboveAfter I revert changes on the router the problem gone. Fortunately I don't have to make Subnet Mask restriction on my project right now, but in the near future I have to.
Have you ever seen this behavior?