Hello,
quick question when i load and run spi_flasher_out into the board after following the instructions, i get an error regarding missing main.c (in pic)
Is it an error that can be ignored? Because the spi flash does run ( I get to flash/erase etc. etc ) and i do get to load both Bootloader and Application from the sdk folder (in my case the profinet example)
I ask because, although the program loads successfully I think the function inside input data task might not be run (regarding the digital input position 1-9 via the rotary controller with different functions) Because changing the rotary controller doesn't do anything to the LCD display/LED when it comes to position 5,6,7,8.
bios : 6_45_01_29
pdk v1.0.3
sdk v2.1.1.2
ccsv6
PS: I also get this other error after SYSTEM-RESET
but read that a HW-Reset and reloading the Initialisation script helps solves that and it did.
Thank you