Hi!
I want to do a mailbox_post inside a function which is called from a uart HWI. I set the mailbox_post timeout to zero but my programs ends when it's doing the mailbox_post() call. When i do the exact same mailbox_post() in a function it is working fine.
Thanks!
Orignial post:
I want to implement a mailbox in my code but it exits when doing mailbox stuff. So i tested the event example but this gives the same result.
When i run the program it prints some stuff and then exits to the loader_exit().
writing message id = 0 val = 'a' ... writing message id = 1 val = 'b' ... writing message id = 2 val = 'c' ... Implicit posting of Event_Id_02 read id = 0 and val = 'a'. Implicit posting of Event_Id_02 read id = 1 and val = 'b'. writer done. Implicit posting of Event_Id_02 read id = 2 and val = 'c'. Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01
I'm using TI-RTOS 2.16.01.14
Thanks!