Hi all,
Today I attempted to program my TM4C129ENCPDT with the mutex example provided in the TI-RTOS for TivaC. It was not modified, only run and an attempted debugging. However, I got the following error: CS_DAP_0 (Error -260 @ 0x0). This has happened on two separate computers, and I am able to connect and debug on my MSP432 board as well as run a driverlib-based program on the TivaC from the same computer. Is this a known issue, or is there something special that I'm not doing for the TI-RTOS based examples?
Thanks in advance!