Hi,
I am new to BLE, so please excuse if there is any basic issues.
I installed CCS and than downloaded the "ble_sdk_2_02_00_31_setup" .
than I created a folder -kk1, and installed in that Folder.
2) I have opened view->Resource explorer.
In that on the top-> I added the kk1.
I am able to see in explorer on right side -> ble_sdk_2_02_00_31. and tirtos_cc13xx_cc26xx_2_18_003.
Question1) what is tirtos_cc13xx_cc26xx_2_18_003 and how is it used? As I am working on sensor I will be using ble_sdk_2_02_00_31?
than I went to ble_sdk_2_02_00_31 -> Examples-->cc2650stk-->sensortag-->ccs.
in that there are :a) sensortag_cc2650stk_app and
b) sensortag_cc2650stk_stack.
Question2) what is sensortag_cc2650stk_stack. for? for me to write applications only sensortag_cc2650stk_app is sufficent right? I do not need any stack right as I am not changing anything?
than for: sensortag_cc2650stk_app
I did step1) import the example to CCS -> Success and green.
than I did step2) I am getting the following Error:
==
**** Build Finished ****
Buildfile generation error occurred..
Product 'com.ti.rtsc.TIRTOSCC13XX_CC26XX' v2.18.0.03 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
==
Question3) what should I do to remove this Error?
=========
When I go to properties:
I see the following Error on the top:
None of the currently selected products include platform support.This project requires pre-3.30 version of XDC tools(or) Additional repository containing the Platform named below.
Question4) what is this error on the top?
In the same location I see Compiler version.
T1V5.2.6 [TI V16.6.0.STS]
TI V16.6.0.STS
Question 5) which one should I select and when to use them?
==
Can you please help me so that I can build a CCS-sensortag on my laptop and also develop applications...