I'm running into a similar problem as detailed in the "TI-RTOS template not visible in Project templates in CCS 5.4" post from a few years ago.
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/288408
I've uninstalled, deleted, and done just about everything else when it comes to TI-RTOS for C2000. My system states that it is installed (see pic), yet it doesn't show in the Project templates and examples area.
I've read through the TI-RTOS 2.16 for C2000 - Getting Started Guide (http://www.ti.com/lit/ug/spruhu3d/spruhu3d.pdf), with no luck other than for me to question if the only way to do this is to create an Example Project using the Resource Explorer in CCS, per Section 3.1.1 of this document. Is this possible using the New CCS Project method as I'm trying to do below in the attached screen capture or do I need to go through the Resource Explorer per the Getting Started Guide?
What am I missing?