• TI thinks resolved

RTOS/TI-RTOS: Cannot get available products window to show anything

Part Number: TI-RTOS

Tool/software: TI-RTOS

CCS Version  Version: 7.1.0.00016  just updated.

This used to work, now not at all

Launch CCSV7 with clean option after update.
Create new Workspace
Project -> New CCS Project
Target MSP430FR5994
Name Test01
Goto
TI_RTOS Examples
Driver Examples
Empty Examples
Empty Project

Next Select TI-RTOS for MSP43X 2.20.0.06
Target:ti.targets.msp430.elf.MSP430X
Platform:ti.platforms.msp430:MSP430FR5994
Build Profile: Release
All the defaults
XDCTools default is 3.32.0.06_core but select 3.5.1.12_core as it is newer.
Finish
Build project
Get errors
Description Resource Path Location Type
error #148: declaration is incompatible with "xdc_Ptr ti_sysbios_BIOS_RtsGateProxy_Proxy__delegate__S(void)" (declared at line 244 of "C:/ti/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/package/BIOS_RtsGateProxy.h") .xdchelp /Test01 line 7482 C/C++ Problem

Select 3.323.0.06_core
Clean and build
No errors this time
Now select empty.cfg to view
No Available Products Window
Select view - Available products window.
Window opens but tells me there is no RTSC configuration b Filke op0en. But have one open empty.cfg
Apparently it doesn't recognize it
Create new RTSC Configuration File from new file menu  file: Same story
Now what?

  • There is a known issue with XDCtools 3.32 and CCS 7.1. You cannot graphically edit the .cfg file. The build should work (which is what you are seeing). The options are
    1. Use 3.32 and edit the .cfg as a text file.
    2. Use 3.50 to edit and then switch to 3.32 to build.

    Todd
  • In reply to ToddMullanix:

    Any idea when the underlying problem will be corrected?
  • In reply to Frank Chambers:

    It turns out that 3.32.00 is okay to use for xGConf and building with CC7.1. Do not use 3.32.01 though. So I should have said
    0. Use 3.32.00 and all is well (you can get it here: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/rtsc/index.html
    1. Use 3.32.01 and edit the .cfg as a text file.
    2. Use 3.50 to edit and then switch to 3.32.01 to build.

    The next TI-RTOS for MSP430 will use XDCtools 3.50. The exact time-frame for the next TI-RTOS release is up in the air. We'll be removing the MSP432 out of TI-RTOS for MSP430 since the MSP432 is supported in the SimpleLink SDK (which has TI-RTOS).

    [edit...fixed link]

  • In reply to ToddMullanix:

    Todd,

    Thanks.  Don't have 3.32.00 and the link is broken

    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/rtsc/index.html)

    Produces the following error message:

    An error occurred while processing your request.

    Reference #132.c734fea5.1493221232.1ca37083

    I do have

    3.50.1.;12_core

    3.2.1.22_core

    3.2.0.06_core

    Compiling gpiointerrupt with the 3.5 version  yields:

    Description Resource Path Location Type
    error #148: declaration is incompatible with "xdc_Ptr ti_sysbios_BIOS_RtsGateProxy_Proxy__delegate__S(void)" (declared at line 244 of "C:/ti/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/package/BIOS_RtsGateProxy.h") .xdchelp /gpiointerrupt_MSP_EXP430FR5994_TI line 7293 C/C++ Problem

    Compiling with 3.2.0.06 yields:

    Clean compile but still need to hand edit the cfg file.

    If you can send me a better link to 3.32.0.0 I will give it a try.

    My CCS is fully updated. A check for updates yields no updates found.

    Starting to feel a pinch. I have finished the upstream part of the project and need to get this part going again.

    Thanks again for your help.

    Frank

  • In reply to Frank Chambers:

    There was an extra ')' at the end...
    software-dl.ti.com/.../index.html
  • In reply to ToddMullanix:

    Todd,
    Sorry for all the bother. The link works to a point. I am getting to the correct page but 3.32.00 is not there.

    XDCTools 3.32
    3.32.01.22 - FOR USE WITH CCS 6.1 (or later) ONLY. See release notes for bugs fixed in this release.
    3.32.00.06 - FOR USE WITH CCS 6.1 (or later) ONLY. See release notes for bugs fixed in this release.

    I have tried the 3.32.00.06 version and it doesn't produce the products panel for the cfg file.
    Plan B? Should I use the jre version even the no jre is recommended for CCS which uses Eclipse

    XDCtools Product Downloads
    Title Description Size
    3.32.00.06 Core (Windows) 3.32.00.06 Core for Windows 57816K
    3.32.00.06 Core (Linux) 3.32.00.06 Core for Linux 64344K
    3.32.00.06 Core (MacOS) 3.32.00.06 Core for MacOS 10.9 64176K
    XDCtools Core without a JRE. Recommended for use within the Eclipse IDE.
    3.32.00.06 Core - JRE (Windows) 3.32.00.06 Core without a JRE for Windows 20976K
    3.32.00.06 Core - JRE (Linux) 3.32.00.06 Core without a JRE for Linux 18584K
    3.32.00.06 Core - JRE (MacOS) 3.32.00.06 Core without a JRE for MacOS 10.9 18784K
    ?
    Thanks
    Frank
  • In reply to Frank Chambers:

    I was omitting the build number (last digit). It is 3.32.00.06 that you want.

    What does your screen look like?

    If it does not have the "Available Products", please open View->Other...->RTSC->Available Projects.

    If it does not have the "Outline", please open View->Outline

  • In reply to ToddMullanix:

    Todd,

    Alreadfy tried that.  Started anew to make sure everything from the correct place.

    Retrived the TMP006 I2C project using resource explorer. Took it from the TI-RTOS for MSP430-v2.20.00.06 tree from Development tools msp-exp430fr5994 driver examples I2C examples I2C TMP006

    Loaded it, used clean and build, opened up the Available products window, loaded the i2ctmp006.cfg file and got the following text in the window "shows modules on the package path of an RTSC project This view is currently empty because there is no RTSC Configuration file open.  i2ctmp006.cfg IS open so should show the tree.

    Checked the PATHS under properties Resource linked resources, all ok, Correct XDCTools 3.32.0.06_core, TI-RTOS for MSP43x 2.20.0.06 OK Compiler Ti v16.9.2 LTS

    Other paths appear to be correct.

    Ideas?

    Frank

  • In reply to Frank Chambers:

    Can you attach a screen-shot of your project? For example

    Also the complete rebuild log. Please attach instead of copy/pasting.

  • In reply to ToddMullanix:

    Todd ,

    Found the log file.  Tried to get the screen shot to you gave up after 20 mins of load time, will try again. Will do screenshot in a seperate reply so you should at least get this

    Thanks

    Frank

    gpiointerrupt_MSP_EXP430FR5994_TI.build.log