Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hello,
I am trying the training material for TI-RTOS and I have problems with the lab session of the hwi module.
I am using Code Composer Studio v7 and the MSP430 FR5994 LaunchPad Development Board.
I will try to toggle the LED by using an example based on driverlib and it works fine. Specifically, I am using Timer_A1 in continuous mode.
I believe that the problem is associated with the definition of the hwi instance in a graphical way. Below is the configuration. I will also test with the value 48 in the interrupt number, which I think is the correct one.
I attach the CCS project:
I hope that you can help me because I am beginning with TI-RTOS and I do not khow what more can I test.
Thanks and regards,
Juan Antonio