Tool/software: TI-RTOS
Is there any limitation in using GateMutexPri with CC13xx with BIOS in ROM. I'm using TI-RTOS for CC13XX and CC26XX v2.21.0.06 with CC1350. I see from the base CFG file below that semaphore priority support is not supported when using BIOS from ROM, and I'm just wondering if a similar limitation my exist for using GateMutexPri.
/* ================ Semaphore configuration ================ */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
/*
* Enables global support for Task priority pend queuing.
*
* Pick one:
* - true (default)
* This allows pending tasks to be serviced based on their task priority.
* - false
* Pending tasks are services based on first in, first out basis.
*
* When using BIOS in ROM:
* This option must be set to false.
*/
//Semaphore.supportsPriority = true;
Semaphore.supportsPriority = false;
-Ruben