I am a newbe to CCS4 RTSC XDC and VOLIB and need some guidance. I would like to run the VAU and TDU on my EZDSP5505 USB stick. I was able to create a project with the neede RTSC components included, the VoLIB C55x V1.0.0 is checked in the Products and Repositories tab of the RTSC tab of the CCS Build propery of my project, so I think I have the context to use the VoLIB in my project. When I look in C:\Program Files\Texas Instruments\volib_C55_1_0_0_1\packages\ti\mas\tdu\test I cannot find a project or anything that resembles a CCS3 or 4 project.
I try to follow the instrunctions on C:\Program Files\Texas Instruments\volib_C55_1_0_0_1\docs\doxygen\html\vau_test_html\index.html but quickly get lost (not a lot of context). It refers to CCS3 and Matlab, neither of which I have.
Can someone share a CCS4 project which builds the VOLIB TDU test package?
Thanks
Rob