This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

WinCE eboot debugging through CCS4?

Champs,

 Is there a way that you can download eboot image through CCS4 and debug?

I am not sure what is the image format generated by wince tools and is there a tool that converts to elf?

I have used CCS for debugging uboot in elf format and looking for a similar mechanism for eboot.

Thanks and regards,

Tony Francis

  • Hi,

    You may upload eboot.nb0 directly to the memory and manualy set the PC to the start address. I did debug the eboot in that way.

    Regards,

    Vitaly

     

  • In reply to Vitaly Andrianov:

    Thanks Vitaly. That was useful.

    As I understand nb0 stands for Raw image format

    bin is as described here: http://msdn.microsoft.com/en-us/library/ee478913(v=winembedded.60).aspx

    With this method, debug symbols will not be there and I cannot see the symbol information (assembly debugging will be tough)

    I saw a tool called Cvrtbin which converts to srecord.

    But CCS doesnt understand srecord right? Any other way?

    regards,

    Tony

  • In reply to Tony Francis:

    Tony,

    As I know SREC format also doesn't have symbol information. I don't know the way of source level debugging the eboot with CCS. I used an eboot.map and corresponding source.cod files for debugging. Of caurse that wasn't very convenient, but worked anyway.

    Regards,

    Vitaly

     

      

  • In reply to Vitaly Andrianov:

    Vitaly,

    It worked and thanks for your help.

    As a side note: Loading eboot to external RAM and then setting the PC did not work as I feel eboot is not stand alone.

    I executed the MLO/XLDR (x-loder) and then loaded and executed eboot both through CCS and then I was able to get the eboot prompt.

    On linux side, uboot is independent of x-loder and I wish wince is also that way.

    I could download through pserial as well, but looks like pserial flash to NAND and but i dont know if there is a way to only download and execute through RAM procedure. Any one knows?

    Thanks and regards,

    Tony Francis

     

     

  • In reply to Tony Francis:

    Tony,

    The MLO has small size and is loaded to the internal RAM. It does all necessary initialization (SDRAM, pinmux and so on) and after that loads eboot or u-boot to the intialized SDRAM. Some SoC have internal RAM big enough for entire eboot or u-boot. I think you are talking about u-boot for that type of SoC. In the case of one step boot loade the u-boot or eboot are responcible for the SDRAM, pinmux and other intialization.

    Any way, if you want to download the eboot to SDRAM through CCS w/o MLO intialization, you have to use a CCS gel file which does all of the intialization.

    Regards,

    Vitaly

        

      

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.