Hi,
there is a problem with the system. the problem is as follows:
When my application draw the screen with picture (say bitmap), the application is ok,but, If the power is off unexpected (I simulated it by cut off the power when the application is running) as the application is running . when I powered the system again , the application will always crashed.
if anyone encountered this problem before?
Hope for your reply!!
best regards!
LIuyan from NovaStar company
nova_liuyan@163.com
What do you mean by powering off the system? Is it a full power cut or putting the board to suspend?
Also please provide the platform you are using, the BSP that is running on it, and more information (log?) regarding the application crash.
Adeneo Embedded Support teamContact us at sales@adeneo-embedded.com