Hello,
I want to know how much memory capacity is needed to run the win CE6.0 in the nand flash for the omapL138 processor.
Regards
Vinoth.
It depends upon what all components are included in the OS design. Sample OS design requires about 15 MB - with Silverlight & IE about 25 MB
thanks
Atul
Hi atul,
I am trying to use the omapL138 EVM kit to drive my custom LCD panel.I am running Windows CE to develop some application to be run on the EVM kit.I have come to know that the OMAP L138 supports LIDD mode for LCD.
My eventual goal is to run WINDOWS CE and the LCD in LIDD mode.(the LCD panel with controller I am using doesn't let me do a raster mode display).
hi atul
Thanks for your response. I want to to know what are the peripherals that are included in the normal os design. whether the executable is also included in that 15mb that you mentioned.
Yes these are sample nk.bin sizes. What WinCE port are you using?
We are using serial port.pls check the full queries above dis and help me hw to do start with dat. and you not mentioned me what are peripherals that included in the os design.waiting 4ur response.
Hi Vinoth,
did you the windows ce port by yourself or did you get it from TI or another company?
Thanks for the information,
Joe
hi joe
Am getting the evm kit from TI.and we are creating our own bsp for that board.
There is an early release of WinCE BSP on OMAP-L138 available for select customers and I was referring to the OS Design in that - it includes pretty much all peripherals. This BSP will be available for wider distribution around July timeframe
What is about OMAP-L137?
Same timeframe
Would it be possible to get also an early release of WinCE BSP for OMAP L137?
Hello Vinoth
I hope you are still in same field.
I have also customized wince over omap l138 with dsp link.
can you help me with developing .exe file for hello word program.
hemant