Hi, All
I have make WL1271 WiFi running well on our DM3730 Board with WinCE 6.0 OS, but Now we want to make it supports Windows Embedded Compact 7.
As we all know, WinCE 6.0 works with wireless zero configuration, but Windows Embedded Compact works with Native wifi architecture, they are different a lot.
Would someone here help me to solve this problem?
Thanks a lot....
Best Regards,
Stephen Zhang
My advice would be stay with CE6 ...unless you have some compelling reason to move to WEC7. Like you need a Silverlight UI or absolutely need ARM7 support. Be prepared for lots of frustration … and much bigger images sizes.
Hi, David Vescovi
Thanks for your reply.
In fact, I need Silverlight UI ,ARMV7 support and RemoteFX support.
Would you help me to move wifi to WEC7?
Thanks
Hi Stephen Zhang
I'm trying to do the same you did, that is migrate from CE6 to 7. However, it doesn't go as smooth as I expected. After changing the sources to fit WEC7, for some reason I get an error message from bscmake.exe which doesn't find files in a temp directory ( which are indeed not there, but I suspect they are in thr_XX where XX changes but there are always .sbr files there )
BSCMAKE: error BK1506 : cannot open file 'C:\Users\WEC7\AppData\Local\Temp\bld_19202\thr_3312\*.sbr': No such file or directory
Did you get the same error? if so, how did you solve it?
Best regards,
Shahal
There is a third parting supporting the WLAN driver for WEC7. They have been notified about the interest in the driver and they should be in touch.
Adeneo Embedded Support teamContact us at sales@adeneo-embedded.com
Hi Stephen
Integrity-Project is license of TI Wifi driver for WEC7: http://www.integrity-project.com/wilink-drivers-and-solutions/
We already have a WEC7 driver with the latest MCP version, much more newer then the driver you have.
Please contact us for more information.
- Elad
- Elad Raz
CTO
www.integrity-project.com
Hi, Shahal
There maybe are comipling errors.
Pls make sure you have closed the antivirius software and firewall, then rebuild again.
Hi,Elad
Thanks.
Would you pls give me some information about the drivers and how to charge?
Best Regards,
Stephen zhang
Integrity has NDIS 5 driver and NDIS 6 driver. Both of them are on top of latest TI driver + FW.
You are more then free to contact us in private email for additional information, pricing and support models.
Are you using a "native WIFI" implementation as Windows Embedded Compact 7 requires or are you using a third party supplicant?
We are using native Wifi for our certification tests.
We also support thrid-party supplicants integrations (and Integrity based supplicant with full CCX support, WiFi direct / SoftAP).