This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am able to build dsplinkk.dll and execute the sample message application(on WinCE 6.0) when i create a folder DSPLINK under $(_WINCE600)\3rdParty\DSPLINK.
Now i wanted to create an application under $( _WINCE600)\PLATFORM\<OMAPL138_BSP>\SRC\APPS\<Sample Application Folder>, for ARM-DSP communication using dsplinkk.dll
I tried copying the sample message application under $( _WINCE600)\PLATFORM\<OMAPL138_BSP>\SRC\APPS\<Sample Application Folder>.
Under <Sample Application Folder>, created two folders gpp and dsp.
Copied the contens from \DSPLINK\dsp\src\samples\message to $( _WINCE600)\PLATFORM\<OMAPL138_BSP>\SRC\APPS\<Sample Application Folder>\dsp\message
Copied the contens from \DSPLINK\gpp\src\samples\message to $( _WINCE600)\PLATFORM\<OMAPL138_BSP>\SRC\APPS\<Sample Application Folder>\gpp\message
Added the dirs and sources files.
When i tried to build it, getting many errors ( mostly syntax errors in .h files )
Would be thankful, for any help or pointers in resolving the problem.
Also any link, to standalone sample application which using dsplinkk.dll for ARM-DSP communication, on WinCE would be helpful.
Regards,
SS