This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[AM335X WINCE7][BSP_WINCE_ARM_A8_02_30_00_Source.exe] UMS(USB MASS Storage) failure

 

I am using AM335X_EVM_15X15BASEBOARD. my sw BSP is BSP_WINCE_ARM_A8_02_30_00_Source.exe.

 

My activesync work well, but UMS(USB Mass storage) work failure. below is uart log debug message:

匓攣Board Type: SKU#00 Using Profile#0 (g_dwBoardProfile=0x1) INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0x8409

Texas Instruments Windows CE EBOOT for AM33x, Built Jan 22 2013 at 15:32:01 EBOOT Version 0.0.1, BSP BSP_WINCE_ARM_A8 02.30.00.01

TI AM33X

ecc type:3 System ready! Preparing for download... INFO: Predownload.... Checking bootloader blocks are marked as reserved (Num = 18)

INFO: Boot configuration found. Boot config Version 3, Signature 1111705159 IsValidMBR: MBR sector = 0x480 (valid MBR) OpenPartition: Partition Exists=0x1 for part 0x20.

>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<< 32a194d4 dc6b -> d4 94 a1 32 6b dc 32a194d4 dd6b -> d4 94 a1 32 6b dd Hit space to enter configuration menu [42] 5...
Hit space to enter configuration menu [1042] 4... Hit space to enter configuration menu [2042] 3... Hit space to enter configuration menu [3042] 2... Hit space to enter configuration menu [4042] 1... Init HW: controller RST SDCARD: requested speed 1000000, actual speed 1000000 SDCARD: requested speed 25000000, actual speed 19200000 BLSDCardReadLogo: cannot open Logo.bmp OEMPreDownload: Filename nk.bin

BL_IMAGE_TYPE_BIN

+OEMMultiBinNotify(0x8feb2378 -> 1) Download file information: ----------------------------------------------------------- [0]: Address=0x80002000 Length=0x03bc94ac Save=0x80002000 ----------------------------------------------------------- Download file type: 1 +OEMIsFlashAddr(0x80002000) g_eboot.type 1 ......................................................................................................................................................................................................................................................................................................................................................rom_offset=0x0. ..ImageStart = 0x80002000, ImageLength = 0x3bc94ac, LaunchAddr = 0x8000b540

Completed file(s): ------------------------------------------------------------------------------- +OEMIsFlashAddr(0x80002000) g_eboot.type 1 [0]: Address=0x80002000 Length=0x3bc94ac Name="" Target=RAM ROMHDR at Address 80002044h Launch Windows CE image by jumping to 0x8000b540...

Windows CE Kernel for ARM (Thumb Enabled) CPU CP15 Control Register = 0xc5387f CPU CP15 Auxiliary Control Register = 0x42 IT IS A GP BOARD
Board Name: A33515BB Board Ver : 1.1A Board Ser : 50114P160081 Board Type: SKU#01 Daughter Board is present DB Board Name: A335GPBD DB Board Ver : 1.1B DB Board Ser : 50114P130081 DB Board Type: SKU#00 Using Profile#0 (g_dwBoardProfile=0x1) +OALTimerInit(1, 24000, 200) --- High Performance Frequecy is 24 MHz--- PID:00400002 TID:00410002 SetOpp to 3 PID:00400002 TID:01350006 ECC TYPE is BCH 8 bit with ELM PID:00400002 TID:01350006 8Bit NAND device PID:00400002 TID:01350006 CM3: input file [\windows\firmware.bin] is 9932 bytes long PID:00400002 TID:01350006 CM3: firmware file read ok! PID:00400002 TID:01350006 +EnableHPOut_PLL fs_ref=48kHz, sample_rate_div=1 (0x00), lVol=0x00, rVol=0x00 PID:00400002 TID:01350006 +TLV320AIC3106CodecConfig::EnableLine1: lVol=0x30 rVol=0x30 PID:00400002 TID:01350006 Cpsw3g_InitializeAdapter: mode=1, port=1, txCh=0, rxChMask=0x01, ActiveCpgmac=1 PID:00400002 TID:01350006 SDHC: CPU revision 0xffffffff PID:00400002 TID:01350006 SDHC host controller initialize: m_fastPathSDIO:1 m_fastPathSDMEM:0 PID:00400002 TID:01350006 -PRU_Init: rc=1 PID:00400002 TID:01350006 CAM3xxOTG::Init DEVCTL 98 PID:00400002 TID:01350006 CAM3xxOTG[1]::FunctionMode(): entering function mode PID:00400002 TID:01350006 CAM3xxOTG::Init DEVCTL 88 PID:00400002 TID:05630002 PVR:getCpuFamily: 5 PID:00400002 TID:05630002 PVR:omapsgxddgpe getCpuFamily: 5 PID:00400002 TID:075B0036 Warning: you are requesting IOCTL_HAL_GET_DEVICE_INFO::SPI_GETPLATFORMTYPE, which has been deprecated. Use IOCTL_HAL_GET_DEVICE_INFO::SPI_GETPLATFORMNAME instead. PID:07590036 TID:075B0036 Total Class Mode is 4 PID:07590036 TID:075B0036 InitUSBSetup Dump PID:07590036 TID:075B0036 ClientName=Mass_Storage_Class PID:07590036 TID:075B0036 Descritpion=Mass Storage PID:07590036 TID:075B0036 InitUSBSetup Dump PID:07590036 TID:075B0036 ClientName=RNDIS PID:07590036 TID:075B0036 Descritpion=Rndis PID:07590036 TID:075B0036 InitUSBSetup Dump PID:07590036 TID:075B0036 ClientName=Serial_Class PID:07590036 TID:075B0036 Descritpion= PID:07590036 TID:075B0036 InitUSBSetup Dump PID:07590036 TID:075B0036 ClientName=USBSER_Class PID:07590036 TID:075B0036 Descritpion= PID:07590036 TID:075B0036 Mode 0: 800x480x32 PID:07590036 TID:075B0036 Check Helper DLL - tcc_dss_setbootrearcaminfo PID:07590036 TID:075B0036 Check Helper DLL - tcc_dss_getbootrearcaminfo PID:07590036 TID:075B0036 ModeChange Current Mode..! PID:07590036 TID:075B0036 ClientName=Serial_Class PID:07590036 TID:075B0036 Descritpion= PID:07590036 TID:075B0036 Setting to Mass_Storage_Class Mode..!!