Hi, All
We have successfully run WinCE 6.0 on AM335X Soc Chip! Anyone who is interested in it, pls give me email......
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, All
We have successfully run WinCE 6.0 on AM335X Soc Chip! Anyone who is interested in it, pls give me email......
And for those interested in testing on the Starter Kit see:
http://am335xskbsp.codeplex.com/
Both CE 6 and WEC7 available.
Hi, All
The websilte link below is prebuilt images for BeagleBone with CHIPSEE Expansion Board(http://www.chipsee.com/beaglebone-exp.html?___store=english&___from_store=default ) running WinCE6.0.
Pre-Images:
https://www.box.com/s/s7bgd5ghpm3htcu4k88w
Have A Try.
Thanks & BR,
Stephen
I am very interesting, please contact with me via besk@163.com
Thanks a lot.
@ phoenixtju : appreciate your work
some how http://www.chipsee.com/beaglebone-exp.html?___store=english&___from_store=default link is broken.
@Nikunj
I am sorry, but the prodcut is EOL.
You can check another link http://www.chipsee.com/best-product/beaglebone-black-expansion-resistive.html
The differences between these products are the LCD panel, the orginal LCD is 800x480, while this one is 1024x
600.
Thanks & BR,
Stephen
Hi phoenixtju,
I really need your BSP.
Could you check your emails, please?
Thank you very much.
Hi, Victor
I have sent you emails.
We talked about the bsp about 1-2 months ago, do you still remember that?
if you have any other questions, pls email to me. My email is phoenixtju@live.cn
Thanks & BR,
Hi phoenixtju,
I sent you about 5 emails since 26-Dec (including the latter reply).
Could you check your spam box?
Thanks
Hi, Matt
Pls give me emaill through dev2013@live.cn
We can disscuss this.
Thanks & Best Regards,
Stephen
I have loaded a 4GB SD card with the MLO, EBOOTSD.nb0 and NK.bin that comes with the Demo package "WEC7 BBB 01.05.00", Also I have formatted the card with Fat32 and 4096 byte sectors (using hp foarmat tool), and I have used the TI SD card utility for flashing the SD card, Also I have pushed the user button before power up,
But noting happens!!!
I tried without TI Utility and made sd card bootable but no results...
when I power the board up the leds won't flash, , So I think it's a boot problem, How can I be sure that the MLO is in the first sector of the SD card?
I have loaded angstrom img succsfuly on BeagleBone Black.
so please consider the issue and give me the procedure corresponding to this.
Regards
aswin pp
Hi phoenixtju,
Thank you for replying. I tried that image files also, but not working for me.
We want to make sd card bootable or sd card partitioning any thing.
I used xp virtual machine and windows 7...
only problems for nk.bin booting, i can boot .img files.
pls help me...
Hi, ASWIN
This image does work well.
I tried it just now.
So, you need to make two things clear.
1. First, you need to make sure your sdcard is bootable.
Or you can try to put MLO and EBOOT files into the sdcard which you can boot linux succesfully. Then you may see the hdmi port for display can show something. If so, the sdcard you used for booting wince is not bootable sdcard.
2. The HDMI needs to be connected before you power on the BBBlack board.
For the image need to read edid from TDA19988 chip. If you do not connect it ,it will take too long to start up.
Best Regards
Hi phoenixtju,
can i use 4gb sd card, and windows 7 as host.
I load sd card with out nk.bin then also its not booting.
I am using hp format tool and can you send me procedure to boot sd card and copy files.
Hi, ASWIN
I think 4GB SDcard can work.
What I say is :
Put MLO and EBOOT into the SDCard which can boot linux succesfully, You did as what I said?
And you connect the HDMI cable with monitor HDMI interface before power on ?
I am interested, pls give me detail informations, thank you! engineering2@zeiger.com.cn