Hi,
We have downloaded the Adeneo Demo Images from their website.
We are using AM335X EVM.
As we are using Windows 7, formatted the SD Card in Windows Explorer.
Modified 0x1BE location in SD Card to 0x80.
Copied MLO, EBOOTSD.nb0 and NK.bin
The EVM shows the below console messages
CCCCCCCCCCCCCCCCCCCCCCCC
Texas Instruments Windows CE SD X-Loader v1.0.0 for AM335x StaterKit - AM33X
Built Jul 4 2014 at 12:51:02
Version BSP_WINCE_ARM_A8 03.01.00.01
open ebootsd.nb0 file
Init HW: controller RST
SDCARD: requested speed 1000000, actual speed 1000000
SDCARD: requested speed 25000000, actual speed 19200000
pBSector Address : 0x4030ADB0
read ebootsd.nb0 file
jumping to ebootsd image
Was anyone able to boot V302 or V310 from AM335X EVM.
I have two EVMs and both of them show the same result.
Any help on this.
Regards,
GSR