PLEASE READ FIRST: TI WinCE Forum Usage Guidelines

 

Welcome to the WinCE for TI OMAP/AM Processors Forum!

This forum is for issues with TI supplied BSP and DVSDK for WinCE on TI’s OMAP35x/DM37x and AM(Sitara) processors (on TI supported EVMs). Before reporting an issue, please try to recreate the issues on TI supported EVM and list the steps, since EVMs are the only platforms on which we can debug.

Before you post:

When reporting an issue or asking a question, please include:

  • Processor you are using
  • BSP version 
  • Platform (EVM or custom board)
  • Steps to reproduce the problem

If the question is related to TI's DVSDK software for WinCE, also include 

  • DVSDK version or component version as applicable.

This forum is NOT for questions about:  

Here are a few more guidelines for using the forum:

  • Please provide tags for your post with any relevant details or keywords to help the overall community (e.g. BSP, WINCE, OMAP35xx, USB etc)
  • If you are satisfied with the answer, please click on the "Verify Answer" button of the answer post. 
  • Create separate posts for unrelated issues

Thanks

 

 

---