All,
Do you have to use new EBOOTXXXX.bin each time you rebuild an OS runtime image or can you stick w/ the ones delivered w/ the BSP package. I'll use BSP 6.13.0 OMAP3503 as an example
BSP - bspdemo_omapwince_06_13_00, comes w/ EBOOTXXXX.bin, NK.bin, XLDRXXXX.bin, and TIEVM3530-XXXX.raw, where XXXX is either NAND, ONENAND, or SD.
When you rebuild OMAP3503 for Debug, there are new 'EBOOTXXXX.bin' files in the \RelDir\TI_EVM_3530_ARMV4I_Debug.
So, can you just use the XLDR + EBOOT (or as its combined into 'TIEVM3530-xxxxxx.raw') from the original BSP 'DEMO' install?
Also, say one wants to use Platform Builder to download/re-flash XLDR or EBOOT - how do you do this? I only see examples of using PB to load NK.bin automatically when you connect and reboot the EVM.
Thanks.