This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bluetooth system requirement

Other Parts Discussed in Thread: CC2564

Hello

I need to install a CC2564 on a Windows CE 6.0 platform, and develop a software on the WinCE to communicate through the CC2564 out to mobile devices. 

My question is: are there system requirements on the Windows CE other than serial connection? I.e. once the CC2564 is installed into the board, using UART, are there additional drivers that need to be installed, or can I control it through my program simply using the serial connection?

Thanks