I have recently got a OMAP4460 Blaze tablet . I followed the 7750.HOWTO_Setup_TI_SDP44XX_EmbeddedCompact.pdf, and built the image using the provided build script CE8_4470_Retail.bat.
I formatted the SD(MicroSD, With Adaptor) card using the HP USB disk storage format tool (As mentioned in the user guide) and copied MLO, ebootsd.raw, eboot.bin, NK.bin and boot.cfg files.
I connected the power cable and the USB (for serial terminal Debuging using UART). Connected the Teraterm (serial port 38400baud.) . Then I inserted the SD card.
When I power up the board i get the below logs(see blue colored text). I am not seeing any logs related to eboot. I also tried with the prebuilt binaries from this link http://fs.adetelgroup.com/dl6885546449 which is provided by adeneo embedded.
I want eboot to see some logs. I am not sure what is the issue here. I wanted to evaluate WEC2013 platform so i purchased this blaze tablet (as the BSP is provided with the installation). No documentation also available like schematics user guide etc. related to the platform.
Texas Instruments Windows CE X-Loader for OMAP4 SDP4470
Built Mar 15 2015 at 20:45:01
General Purpose processor
ES 1.0
load ebootsd.raw
### high-capacity card
successfully read eboot