Hi there, I used the existing supported BSPs for OMAP3530 family provided during WEC7 installation. The build was successful on this case. But I am unable to boot the device through SD card.
Then, I downloaded the actual BSPs from Adeneo site and I am facing the issue that oal.h file was not found. Actually TI is recommending to use the BSPs download from Adeneo instead of which comes built-in with WEC7. As indicated in microsoft forum, I checked the DIRS file (to remove the oal.h was not found error) in C:\WINCE700\platfrom folder and it presents and I simply deleted. Also, I couldn't see oal.h file in platform\common folder either. Can you please guide me where the dirs file should be present (and what content should it has) and how to get the oal.h file to complete the build successfully.
Once I remove that dirs file then, I could see the following build msgs.
C:\WINCE700\build.log(32370) : Error: Could not find file 'C:\WINCE700\OSDesigns\OSDesign5\OSDesign5\RelDir\EVM_OMAP3530_ARMV7_Checked\oal.exe' on disk {log="C:\WINCE700\build.log(32370)"}
C:\WINCE700\build.log(32373) : Error: failed setting line {log="C:\WINCE700\build.log(32373)"}
C:\WINCE700\public\common\oak\misc\makeimg.proj(688,5): error MSB3073: The command "romimage C:\WINCE700\OSDesigns\OSDesign5\OSDesign5\RelDir\EVM_OMAP3530_ARMV7_Checked\ce.bib " exited with code 1. {log="C:\WINCE700\build.log(32374)"}
C:\WINCE700\public\common\oak\misc\makeimg.proj(688,5): error MSB3073: The command "romimage C:\WINCE700\OSDesigns\OSDesign5\OSDesign5\RelDir\EVM_OMAP3530_ARMV7_Checked\ce.bib " exited with code 1. {log="C:\WINCE700\build.log(32381)"}
BLDDEMO: ERROR: Error(s) in makeimg phase. See C:\WINCE700\build.log for details. {log="C:\WINCE700\build.log(32388)"}
BLDDEMO: BUILDMSG: BldDemo ended at 17:16:00.94 on Tue 07/07/2015 (exit code 1)
BuildLogs: BUILDMSG: Exiting: BldDemo1.bat -q (result code 1).
BuildLogs: BUILDMSG: C:\WINCE700\build.log
BuildLogs: BUILDMSG: C:\WINCE700\build.out
BuildLogs: BUILDMSG: C:\WINCE700\build.wrn
BuildLogs: BUILDMSG: C:\WINCE700\build.err
Please help to resolve this build errors.
Thanks and Regards,
Karthick