Hi,
I am using OMAP3530 eval board for WEC7 environment. I have done the build in release mode with KITL and kernel debugger enabled. But, I am not clear from the 'BSP_WINCE_ARM_A8_User_Guide.pdf' how to connect the ethernet port. Its saying the Connect the EVM3530 Ethernet to the same subnet as the Host PC. How to do this and establish a connection to flash the image. Am I need to connect a ethernet cable directly connected to My development PC to the target device...in this case what should I provide the details of IP address, Mask, router and DHCP should enabled or not?? please clarify.
Thanks and Regards,
Karthick