Hi,
I am working for AM/DM37x platform on Windows EC7. I am using "BSP_WINCE_ARM_A8_02_30_00_Source" as AM37x BSP. I need to take out the gpio's 148 to 151 for our development purpose. But these pins already used for UART1. To use these pins as gpio's I did the following changes in bsp_padcfg.h file;
//#define UART1_PADS \
//PAD_ENTRY(UART1_TX, INPUT_DISABLED | MUXMODE(0)) \
//PAD_ENTRY(UART1_RX, INPUT_ENABLED | PULL_RESISTOR_ENABLED | PULLUP_RESISTOR | MUXMODE(0)) \
//PAD_ENTRY(UART1_RTS, INPUT_DISABLED | MUXMODE(0)) \
//PAD_ENTRY(UART1_CTS, INPUT_ENABLED | PULL_RESISTOR_ENABLED | PULLUP_RESISTOR | MUXMODE(0)) \
and added as gpios in the following code;
#define GPIO_PADS_37XX \
PAD_ENTRY(UART1_TX, INPUT_ENABLED | MUXMODE(4)) /* GPIO 148: TRF7970 irq by KPH */ \
PAD_ENTRY(UART1_RX, INPUT_ENABLED | PULL_RESISTOR_ENABLED | PULLUP_RESISTOR | MUXMODE(4)) /* GPIO 151: TRF7970 EN by KPH */ \
PAD_ENTRY(UART1_RTS, INPUT_DISABLED | MUXMODE(4)) /* GPIO 149: TRF7970 MOD by KPH */ \
PAD_ENTRY(UART1_CTS, INPUT_ENABLED | PULL_RESISTOR_ENABLED | PULLUP_RESISTOR | MUXMODE(4)) /* GPIO 150: TRF7970 ASK/OOK by KPH */ \
Please let know that this change itself is enough or should I modify in other files too. Becuase I am seeing the UART1_PADS used in other files also. Should I comment those....
Please share your valuable thoughts.
Regards,
Karthick