Hi,
I use AM37x EVM along with Windows EC7 for the development driver for one of the device.
I developed the driver and modified required registry file, DIRS, platform.bib, sources files for that driver.
Developed as built-in driver.
But when I gave 'build solution' or 'rebuild solution' it generates the OS image.
But if I give 'sysgen' or 'clean sysgen' in Advanced build commands, I get the following error.
BUILD: [01:0000000056:ERRORE] Error(s) in directory "D:\WINCE700\3rdParty\dvsdk_wince_01_11_00_02\".
BUILD: [01:0000000057:ERRORE] prelink.bat failed - rc = 4.
Please share your thoughts if any.
Regards,
Karthick