Hi,
I use omap3530 + windows ec7 for the development.
Also using BSP_WINCE_ARM_A8_02_30_00_Source.
I need to take off the MMC2 data lines 0-3 as GPIOs. For this I did the configuration changes in bsp_padcfg.h file as followed;
PAD_ENTRY(MMC2_DAT0, INPUT_DISABLED | PULL_RESISTOR_DISABLED | MUXMODE(4)) /* GPIO 132: */ \
PAD_ENTRY(MMC2_DAT1, INPUT_ENABLED | MUXMODE(4)) /* GPIO 133: */ \
PAD_ENTRY(MMC2_DAT2, INPUT_DISABLED | PULL_RESISTOR_DISABLED | MUXMODE(4)) /* GPIO 134: */ \
PAD_ENTRY(MMC2_DAT3, INPUT_DISABLED | PULL_RESISTOR_DISABLED | MUXMODE(4)) /* GPIO 135: */ \
And using GpioTest code to toggle the gpios.
There seems to be any changes in the states of pins even I scoped it through. Is there any configuration settings missing here... please let know.
Regards,
Karthick