HI
Am using omapL138 with win ce 6.0 os.
i cant able to attach device. its showing the
error message that cant locate
the run time image file.
I created the clone bsp and i choose the release in the configuration manager
and i enabled the kitl and vmini in the boot menu.I cant able to get the nk.
bin when i build.am getting these errors. but i can see my device in target--
the run time image file.
I created the clone bsp and i choose the release in the configuration manager
and i enabled the kitl and vmini in the boot menu.I cant able to get the nk.
bin when i build.am getting these errors. but i can see my device in target--
>connectivity
options.
regcomp: Error:
InitRegistry FAILED on or near line 870 of C:\WINCE600\
OSDesigns\test\test\RelDir\FREON_NEW_ARMV4I_Release\reginit.ini.
makeimg:
FATAL ERROR: Command returned non-zero exit code 1 (dec).
makeimg:
FATAL ERROR: Command returned non-zero exit code 1 (dec).
test - 3
error(s), 0 warning(s)
Thanks
vinoth.