Hello
While am running to make run time image am getting these errors.
This is the error mess am getting while i trying to build my win ce.
BUILD:
[01:0000000156:INFO ] makefile.def: Including C:\WINCE600\public\
common\oak\misc\Sources.default
BUILD:
[01:0000000157:INFO ] makefile.def: BUILDROOT is C:\WINCE600\PLATFORM\
COMMON
BUILD:
[01:0000000158:INFO ] makefile.def: Including C:\WINCE600\PLATFORM\
COMMON\sources.cmn
BUILD:
[01:0000000159:ERRORE] C:\WINCE600\public\common\oak\misc\makefile.def
(156)
: U1023: syntax error in expression
BUILD: [01:0000000160:INFO ]
Stop.
BUILD: [01:0000000161:ERRORE] NMAKE.EXE WinceTargetFile0 -i -c
BUILDMSG=Stop.
BUILDROOT=C:\WINCE600\PLATFORM\COMMON CLEANBUILD=1
NOLINK=1 PASS0ONLY=1
failed - rc = 2
Can any body tell these
are the lines in makefile.def:
154 # Include the developer supplied
file that defines the TARGETNAME,
LINE NO: 155 # TARGETTYPE and
SOURCES macros.
LINE 156: #
158 #
Local variable which gets set to the tree being
built currently
159 WINCETREE=$(_CURSLMTREE)
can any body
tel what to correct in these..
Regards
Vinoth.