Hello

 

When i try to run the win ce using tera term am getting the following prob that cause my remote display not working.

I already enabled the kitl in target-->>>conn options-->conf settings and
also in the project prop build option i enabled the kitl i dont know what
else i want to make a change.

Pls tell to get rid of this problem.

This is the tera term message which i got

 

 

Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x80000000  Length=0xF2C918  Name="" Target=RAM
ROMHDR at Address 80000044h
Image Start .......: 0x80000000
Image Size ........: 0x00f2c918
Image Launch Addr .: 0x80001000
Image ROMHDR ......: 0xc0da8a00
Boot Device/Type ..: 2 / 1
Got EDBG_CMD_JUMPIMG
Got EDBG_CMD_CONFIG, flags:0x00000000
ADEO: Launch Windows Embedded CE by jumping to 0xc0001000...
Windows CE Kernel for ARM (Thumb Enabled) Built on Oct 20 2009 at 18:39:19
VBridge:: built on [Jun  1 2010] time [17:50:11]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0xA0F6F820] to [0xA0F73820].
Rx buffer [0xA0F73840] to [0xA0F77840].
VBridge:: NK add MAC: [0-8-EE-3-B0-11]
Connecting to Desktop

!Unable to establish KITL connection with desktop!
VBridge:: built on [Jun  1 2010] time [17:50:11]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0xA0F6F820] to [0xA0F73820].
Rx buffer [0xA0F73840] to [0xA0F77840].
VBridge:: NK add MAC: [0-8-EE-3-B0-11]
Connecting to Desktop

!Unable to establish KITL connection with desktop!
!KITLRegisterDfltClient: Fail to initialize KITL


Vinoth.