Processor: OMAP 3530
BSP version: TI_EVM_3530 - 6.13.00
Platform: EVM
I am developing a UVC client driver. since this BSP doesn't supports Isochronous transfer type I have configured the endpoint as bulk endpoint. Max packet size is congfigured as 512 bytes for high speed and Video streaming is successful and host device application is able to shoe the video frames send by the device.
I have enabled the DMA of musbfn (PDD) driver by assigning EnableDMA = 1 in musbfn driver registry.
I have enabled double buffirng also
I have modified following code line in UfnPdd_InitEndpoint function to enable the doulble buffing case EP_TYPE_BULK: OUTREG8(&pGenRegs->TxFIFOsz, (MUSB_FIFOSZ_512_BYTE | (1<<4))); But the problem is that, if I enable the double buffing as shown above, video is streaming but the following error is occuring, "!!! ERROR => PreDmaActiviation wrong for EP 2, state 1" and after some time exception is occureing and video streaming is aborted. Here my question is: 1. The way of enableing the double buffing is right or should I enable some more things? 2. Can we enable DMA and Double buffering at a time? Thanks Subbarao.
I have modified following code line in UfnPdd_InitEndpoint function to enable the doulble buffing
case EP_TYPE_BULK:
OUTREG8(&pGenRegs->TxFIFOsz, (MUSB_FIFOSZ_512_BYTE | (1<<4)));
But the problem is that, if I enable the double buffing as shown above, video is streaming but the following error is occuring,
"!!! ERROR => PreDmaActiviation wrong for EP 2, state 1" and after some time exception is occureing and video streaming is aborted.
Here my question is:
1. The way of enableing the double buffing is right or should I enable some more things?
2. Can we enable DMA and Double buffering at a time?
Thanks
Subbarao.