I have implemented OMAP35x 6.13.00 SDK using the ddge_neon files.
I get the following omap_optblt.cpp/DumpParms() values:
Dst(72 (192 bytes) x 72)=(0, 0) - (72, 72), fmt=4 (16 bpp)
Src(72 (288 bytes) x 72)=(0, 0) - (72, 72), fmt=6 (32 bpp)
solidColor=0xFFFFFFFF
bltFlags=0x00000010
rop4=0x0000CCCC
xPositive=1, yPositive=1
pLookup=0x00000000
pConvert=0xC08AD684
iMode=0x00000001
blendFunction=0x01FF0000
This is expected, but once I return from the call to function AlphaBlendpBGRA32toRGB16() my .png file that has a tranparent alpha layer is not being displayed transparent.
Please help.
Paul