Hi,
I cannot boot correctly in Debug Mode.
I enabled KITL and kernel debugger on Build Options menu, and set BSP_NOETHERNET environment variable to disable Ethernet NDIS miniport driver that interferes KITL communication. I downloaded the OS image (95.9MB) to the target board (TMDSEVM3530) and tried to boot the OS. But Platform Builder (PB) requires some files and I cannot boot it correctly. Below is what I saw and did after PB downloaded the image to the board.
1. "tcsncpy_s.inl" is required by PB, so I selected this file located in C:\\Program Files\Microsoft Visual Studio 9.0\VC\crt\src.
2. "devpnp.c" is required by PB, but this file doesn't exist in C:\\, so I select "cancel" to skip.
3. "bkist.cpp" is required by PB, but this file doesn't exist in C:\\, so I select "cancel" to skip.
4. "thread.c" is required by PB, so I selected this file located in C:\\Program Files\Microsoft Visual Studio 9.0\VC\crt\src.
5. "gwe_s.cpp" is required by PB, but this file doesn't exist in C:\\, so I select "cancel" to skip.
6. "input.c" is required by PB, so I selected this file located in C:\\WINCE700\public\wceshellfe\oak\ctlpnl\intl2.
7. "crtsupp.cpp" is required by PB, but this file doesn't exist in C:\\, so I select "cancel" to skip.
8. "fscall.c" is required by PB, but this file doesn't exist in C:\\, so I select "cancel" to skip.
9. "First-chance exception in KERNEL.DLL. (0xC0000005: Access Violation)" dialog is appeared, then I select "OK".
10. "Pass exception on to the program being debugged? Will default to 'Yes' if dialog disabled" dialog is appeared, then I select "Yes".
11. "First-chance exception in MUSBOTG.DLL. (0xDFFF0123: unnamed)" dialog is appeared, then I select "OK".
12. "Pass exception on to the program being debugged? Will default to 'Yes' if dialog disabled" dialog is appeared, then I select "Yes".
13. OS doesn't boot and PB downloads the image to the board again.
The memory allocation in config.bib is below.
MEMORY
; Name VA Length Type
ARGS 84000000 00001000 RESERVED ; 4K
#if (defined BSP_DSPLINK || defined BSP_TI_DVSDK)
IF BSP_SDRAM_BANK1_ENABLE
NK 84001000 063FF000 RAMIMAGE ; 100MB - 4K
DISPLAY 8A400000 01000000 RESERVED ; 16MB
CMEM_DSP 8B400000 02800000 RESERVED ; 40 MB
RAM 8DC00000 06400000 RAM ; 100MB
ELSE
What causes this problem?