• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » WinCE » WinCE forum » All Tags » 3530
Share
WinCE
  • Forum

Browse by Tags

WinCE

Welcome to the WinCE Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
3530
  • A8 bsp 010100
  • AM/DM37x
  • ARM-A8 WINCE BSP
  • BSP
  • bsp 6.15.00 omap3530 wince6
  • DM3730
  • OMAP
  • OMAP 3530
  • OMAP EVM BSP WinCE
  • omap3530
  • omap3530 wince7
  • OMAP35x
  • OMAP35xx
  • OMAP35xx EVM
  • OMAP35xx EVM BSP
  • WINCE
  • wince BSP
  • WINCE BSP ARM A8
  • WINCE BSP OMAP3530
  • WinCE Compact 7
  • WINCE OMAP3530 BSP
  • WinCE OMAP35x TPS659xx
  • WINCE7
  • Windows CE
  • WindowsCE
Related Posts
  • Forum Post: WinCE BSP 6.14 SD/MMC Performance

    phoenixtju phoenixtju
    Good Day, Everybody. We are now evaluating OMAP3530 SD/MMC Read/Write Performance based on WinCE BSP 6.14, Bsquare provides a document that says SD/MMC Read/Write performance is improved but no performance data to show. Is there some body test it and how to test the performance correctly? Now I just...
    on Jun 12, 2010
  • Forum Post: Re: back to back uSD card file reads

    MPope MPope
    Sorry it's taken me a while to get back to this - other fires. So I've done my best to try the 1x only FileIoInit: This is what I get: ****************** FileIoInit 1x ************************** BootDevice(4) BootDevLoc(4809c000) BLSDDwnld: FN: nk.bin FN2DIR F-OPEN...
    on Aug 21, 2010
  • Forum Post: Re: back to back uSD card file reads

    MPope MPope
    OK - you guys may color me daft. I was going back through my code and I found that I left in some test code that did a reset of the SD controller. Once I took this out - the 1x - FileIoInit method worked. I give much praise and thanks to that suggestion as it worked as advertised. Thank you...
    on Aug 23, 2010
  • Forum Post: How to use the SDMA drive of OMAP3530

    yuantai luo yuantai luo
    In% WINCE600 \ PLATFORM \ TI_EVM_3530 \ SRC \ DRIVERS \ SDMAPROXY path, Able to use SDMA driver for memory copy, to improve CPU utilization。 When I created the SDMA stream driver file, I first used the "IOCTL_SDMAPROXY_CONFIG" control command for DMA configuration, and then apply for...
    on Oct 30, 2010
  • Forum Post: GPIO problem..

    gang luo gang luo
    hi,sir, could you help me to check, here is my problem: i want to set the GPIO 156 to high,below is my souce code : DWORD g_gpioaudioenable=156; DWORD PinMode=1; DWORD dwMode[2] = {g_gpioaudioenable, GPIO_DIR_OUTPUT}; HANDLE g_hGpio = CreateFile(GPIO_DEVICE_NAME, 0, 0, NULL, 0...
    on Nov 16, 2010
  • Forum Post: Re: mmc1 boot problem on omap3530

    Huai Hellen Huai Hellen
    Hi, Jatin You are right, I use sd2 slot on my custom board, the bsp version is 6.14.01 I undef the macro MMCHS1_VDDS_WORKAROUND in in the file OMAP35XX_TPS659XX_TI_V1\inc\sdhc.h, but it does not make any difference. The level shifter I used is tx0106, and what I cleared is that there are two...
    on Nov 22, 2010
  • Forum Post: Logic PD Zoom OMAP35x Development Kit_Booting Issue

    Thomas CN Thomas CN
    Hello, Can any one help on below issue? We use Logic PD Zoom OMAP35x Development Kit. The OMAP processor is not loading Win CE image on power up. It loads the LoLo and runs idle thread. It is able to load the Win CE image if load command is issued through LoLo. By default the boot priority is for...
    on Feb 7, 2011
  • Forum Post: error LNK2019

    yuxin du yuxin du
    BUILD: [01:0000017870:PROGC ] Linking D:\WINCE600\platform\EVM_OMAP3530\target\ARMV4I\retail\kitl.dll BUILD: [01:0000018191:ERRORE] bspcfg.lib(bspcfg.obj) : error LNK2019: unresolved external symbol MmUnmapIoSpace referenced in function BSPGetNANDECCType BUILD: [01:0000018192:ERRORE] bspcfg.lib...
    on Mar 11, 2011
  • Forum Post: no serial output messages of NK.bin after I booted omap3530 from SD card

    Lizhe Liu Lizhe Liu
    Dear all: Recently I have compiled NK.bin use based on the WINCE BSP version----TI_EVM_3530 , but there is no serial output messages of NK.bin after I booted omap3530 from SD card to my own omap3530 board. Some messages before jump to NK.bin are as follows: BL_IMAGE_TYPE_BIN Download...
    on Mar 29, 2011
  • Forum Post: How to compile PowerVR samples for Windows Embedded Compact 7

    Lizhe Liu Lizhe Liu
    Hi, I am a new guy on Windows Embedded Compact 7, and try to make it running on TI EVM3530. Now my NK can work successfully. So I try to test PowerVR samples for Windows Embedded Compact 7. But the application fails down, and the EGL BAD DISPLAY error is generated. Can someone describ excat way...
    on May 27, 2011
  • Forum Post: SMSC9221 chip reset and recovery

    Zack Zadecki Zack Zadecki
    Hi, We've created a board with OMAP 3530 (3730 in next revision) processor and the SMSC9221 chip. We use WinCE 6.0 (we plan to move to 7.0), and the TI BSP has a driver for it (actually for 9118, but it should be compatible). Once a while, in very specific circumstances, we lose the Ethernet...
    on Jun 28, 2011
  • Forum Post: Windows Embedded Compact Framework 7 - Silverlight compatibility problem

    Zack Zadecki Zack Zadecki
    Hi, I've installed WinCE 7.0 with the A8_02_00_00 TI BSP and using this environment I'd like to test a Silverlight 3 project we have. This project (solution) was created using Expression Blend 4 (with Silverlight 3 option), but it can be successfully open also in Expression Blend 3. After...
    on Jul 1, 2011
  • Forum Post: CPEN on USB3320 driving USB power

    Zack Zadecki Zack Zadecki
    Hi, We have a custom board with one of two processors: 3530 or 3730. The earlier ones were made with 3530, and the latest ones - with 3730. With both solutions we have the USB3320 chip managing the EHCI USB port. In the latest release we’ve added chips switching (on/off) the power signal to...
    on Aug 2, 2011
  • Forum Post: Re: DVFS issue

    Carsten Hansen Carsten Hansen
    Just wanted to add my voice as we are seeing similar issues. We are running CE 7.0 (WEC7) on a custom 3503 board. Our BSP is based on 6.15. With DVFS enabled our device had a tendency to lock up randomly, sometimes after an hour of operation but in some cases after several days. After disabling...
    on Feb 10, 2012
  • Forum Post: Silverlight will not run on WEC7 with 2.0 BSP on OMAP3530

    Fuzzkap Fuzzkap
    I am currently working on building the 2.0 BSP (BSP_WINCE_ARM_A8_02_00_00_Source) for a platform using the OMAP3530 (beagleboard rev. c3) with WEC7 (completely updated as of yesterday). The BSP was given minor adjustments to support the beagleboard's DVI and USB-Host features. Currently, everything...
    on Jan 20, 2012
  • Forum Post: How to startup LCD in landscape on Mistral EVM3730 board with WINCE7 ?

    Thomas RETAIL Thomas RETAIL
    Hello, I want to modify the orientation of LCD on startup (not using rotate.exe command). Actually, start in portrait and I want to display in landscape mode. I use WINCE700 and OMAP3730 processor. Which file I must modify to do it ? Thanks for answers, Thomas RETAIL.
    on Feb 17, 2012
  • Forum Post: Technexion's TAO3530 720p cannot display on Samsung TV and Philips 55PFL6606

    Kwang Wee Sim Kwang Wee Sim
    Dear all, I am using Technexion's TAO3530 (OMAP3530 processor) with Wince6.0 R3. The BSP is provided by Technexion as it is without support, I think it is because they probably dont't do the video driver part in the BSP. This board is configured for 720p but for Philips 55PFL6606 and many...
    on Apr 25, 2012
  • Forum Post: OMAP3530 POP Memory Organization

    Bill Derby Bill Derby
    Hello, I have a Embest DevKit8000 with a OMAP3530DCUS chip on it. The Win CE 6.0 R3 BSP supplied by the vendor (Embest) is a rather old and buggy (Bsquare 6.09) and I can only get my builds to work with the memory configured with 128Meg of SDRAM. I have everything running on this unit in a release...
    on May 4, 2012
  • Forum Post: file system and datastorage

    sab nad sab nad
    I am trying to implement persistent storage for evm3530 in win ce 6.0 R3.Every reboot, files which are created in the desktop are wiped out.how to fix this issue.
    on Jun 6, 2012
  • Forum Post: Automation of NAND programming using FLASH v1.6.0.0 utility

    Mahesh Hooli Mahesh Hooli
    Hello All, We are using FLASH v1.6.0.0 utility for programming the NAND (for flashing the WinCE image onto NAND). We are flashing it using through USB. Is there any options to make run these FLASH v1.6.0.0 utility commands using DOS prompt? In production, we would like to automate the flashing...
    on Jul 12, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use