• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » WinCE » All Tags » A8 bsp 010100
Share
WinCE
  • Forum

Browse by Tags

WinCE

Welcome to the WinCE Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
A8 bsp 010100
  • .bin loading error
  • 1280x720
  • 3517
  • 3530
  • 3530 Win CE
  • 3730 WinCE Compact 7 interrupt
  • 6.14BSP
  • Adeneo
  • Adeneo BSP
  • AM/DM37x
  • ARM-A8 WINCE BSP dm3730
  • h
  • omap3 evm 35x 3530
  • omap3530
  • WINCE
  • WinCE OMAP35x TPS659xx
Related Posts
  • Forum Post: why disable drift guard property for dpll in BSP version A8 01 01

    Huai Hellen Huai Hellen
    Hi, all I compare the source code between bsp A8010100 and A8010000, find that in bsp A8010100, disabled the drift guard property ( dpllInfo.driftGuardEnabled = FALSE). Could someone tell me the reason? Thank you!~
    on Mar 4, 2011
  • Forum Post: The problem of the quiescent Current on evm3530(Tps65930) based of sdk A8 01.01.00

    Edward Qing Edward Qing
    Hi, All When the system is suspend,the quiescent current of tps65930 will be more than 8mA. 1. How to reduce this value? 2. when the system is suspend, Can I shut down the HFCLKOUT of TPS65930 ? And how to do that ? Thanks & Best Regards, Edward Qing
    on Apr 1, 2011
  • Forum Post: Hang problem when switching UART debug port from UART3 to UART2

    Luan Le Luan Le
    Hello, From Wiki page WinCE-TIBSP FAQ, it is possible to use UART1/2 for Serial debug message by changing the debugUartCfg structure inside SRC\BSP_COMMON\BSPCFG\bspcfg.c In the debugUartCfg structure of the original EVM_OMAP3530 BSP, I changed the "dev" value from OMAP_DEVICE_UART3 to...
    on Apr 27, 2011
  • Forum Post: Technexion's TAO3530 720p cannot display on Samsung TV and Philips 55PFL6606

    Kwang Wee Sim Kwang Wee Sim
    Dear all, I am using Technexion's TAO3530 (OMAP3530 processor) with Wince6.0 R3. The BSP is provided by Technexion as it is without support, I think it is because they probably dont't do the video driver part in the BSP. This board is configured for 720p but for Philips 55PFL6606 and many...
    on Apr 25, 2012
  • Forum Post: EVM3530 GPTimer10 and PWM

    yuanjun ren yuanjun ren
    Hi,all I use the TI BSP_WINCE_ARM_A8_01_00_03 for Windows embedded compact 6 running on an Evaluation Board EVM3530 with the TI Processor DM3730 . Now I want to generate a PWM Signal with the GPTimer10 and output it over the GPIO-PAD GPMC_nCS5 in muxmode 3. who can give me an example to use GPTimer10...
    on May 27, 2012
  • Forum Post: DM3730 and PWM_10

    yuanjun ren yuanjun ren
    platform: DM 3730 os:wince 6.0 BSP:BSP BSP_WINCE_ARM_A8 1.01.00.03 Now I want to generate a PWM Signal with the GPTimer10 and output it over the GPIO-PAD GPMC_nCS5 in muxmode 3. but no pwm signal was generated, who can give an advice to me ? My code listings as follows. BOOL EnableDeviceClocks...
    on May 28, 2012
  • Forum Post: RE: EVM3730 GPTimer10 and PWM

    yuanjun ren yuanjun ren
    Hi, DavidVescovi Thank you very much! could you tell me how to carry out PulsPulse-Width Modulation e-Width Modulation Pulse-Width Modulation , i.e. which register can I modify, TLDR, TMAR or TTGR.
    on Jun 1, 2012
  • Forum Post: Date/Time reset after 49.7 days

    Zack Zadecki Zack Zadecki
    All, We have an interesting problem with one of our machines (It is running Windows CE 6.0, and DM3730 processor). After 49.7 days of work, the system time/date was reset, but not to the initial one, just to time and date of the previous reset of the machine. Basically it was reverted by 49.7 days...
    on Jun 12, 2012
  • Forum Post: Question on ov5640

    yuanjun ren yuanjun ren
    Hi,all platform: OMAP3530 os:wince 6.0 BSP:BSP BSP_WINCE_ARM_A8 1.01.00.03 camere: OV5640 In my camera driver, When I use 2 - megapixel to capture image , the ov5642 is ok, but I change the pixel format as 5- megapixel ,It does not work . My application is programmed by Directshow.when the mediacontrol...
    on Jun 20, 2012
  • Forum Post: Unable to connect to KITL present on WinCE-BSP target to download and debug application

    Bruce Bassett Bruce Bassett
    I have added TCP/IP and KITL support to my OS Design for the AM335x EVM as described in http://processors.wiki.ti.com/index.php/WinCE-BSP_ARM-A8_Quick_Start_Guide#KITL_Configuration . As I have a point-to-point connection to a NIC on my PC, I hit <space> during the boot and am able to configure...
    on Jul 2, 2012
  • Forum Post: LCD rotation and VRFB

    yuanjun ren yuanjun ren
    Hi,all BSP:BSP_A8_01_01_00 PLATFORM:DM3730 Camera :0v5642 Why my LCD rotation must enable VRFB,otherwise LCD rotation fail. but my camera preview does not work when BSP is built with VRFB enabled. what is the reason?
    on Jul 5, 2012
  • Forum Post: RE: LCD rotation and VRFB

    yuanjun ren yuanjun ren
    I find a passage in the WinCE-BSP ARM-A8 User Guide- “ Preview does not work when the BSP 1.x is built with VRFB enabled and if you dont have the CE6 Nov 2010 monthly update installed on your setup. The Nov 2010 CE6 monthly update fixes the stride issue and Preview will work with VRFB enabled after...
    on Jul 5, 2012
  • Forum Post: Automation of NAND programming using FLASH v1.6.0.0 utility

    Mahesh Hooli Mahesh Hooli
    Hello All, We are using FLASH v1.6.0.0 utility for programming the NAND (for flashing the WinCE image onto NAND). We are flashing it using through USB. Is there any options to make run these FLASH v1.6.0.0 utility commands using DOS prompt? In production, we would like to automate the flashing...
    on Jul 12, 2012
  • Forum Post: RE: LCD rotation and VRFB

    yuanjun ren yuanjun ren
    Hi, Adeneo Embedded support tea m Thank you for your answer, there is a Sentencein your answer-----" we observe when using high resolution camera streams or selecting DVI with a high resolution display output. ",what are the high resolution camera stream and high resotution display? My LCD...
    on Jul 13, 2012
  • Forum Post: Trying to bring up WinCE 7 eboot on a Sitara AM3517 from 8-bit NAND flash

    Andreas Geisreiter Andreas Geisreiter
    Hi, I have problems to start eboot with 8bit NAND Flash. Everithing works fine up to the call of "memcpy(pData, (BYTE*)pDevice->pFifo, FIFO_THRESHOLD)" in the function NAND_Read(). For 8bit NAND FLash support I have changed the source code lines #define WRITE_NAND(x,y) OUTREG16(x,y...
    on Jul 27, 2012
  • Forum Post: DM3730 WinCE6 with eMMC 4.4

    yuanjun ren yuanjun ren
    Hi,all Processor : DM3730 BSP version :wince- A8 bsp 010100 Platform (EVM or custom board): Custom board Steps to reproduce the problem : Can't recognize emmc 4.4 (16G) iNand Can TI wince6.0 BSP support emmc 16G iNand ? How can I driver the iNand?
    on Sep 20, 2012
  • Forum Post: RE: BSP Support for Managed Nand (eMMC)

    yuanjun ren yuanjun ren
    Hi, DavidVescovi your inand is 8bit bus-width, can it support 16G inand?
    on Sep 20, 2012
  • Forum Post: RE: BSP Support for Managed Nand (eMMC)

    yuanjun ren yuanjun ren
    Hi, DavidVescovi I encountered the same problem about eMMC nand, could you share your solution?
    on Sep 21, 2012
  • Forum Post: DM3730 can not reset from sd card

    yuanjun ren yuanjun ren
    Hi,all platform:DM3730 OS: WINCE 6.0 A8 bsp 010100 power manager: TPS65930 My custom board can boot from sd card, but It can not reset from sd card. what is the reason? hardward or software?
    on Oct 9, 2012
  • Forum Post: Urgent probem! why GPIO APIs like GPIOSetBit or GPIOClrBit need so much time to toggle

    Jun LI2 Jun LI2
    Hi , I encountered one puzzling probem while using GPIO functionality on platforms of OMAP3730 WINCE. The issue is that APIs like GPIOSetBit() or GPIOClrBit would take several microseconds to take effect and I am wondering why the time should not be so long. It seems the clock gate settings to...
    on Dec 6, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use