• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » WinCE » All Tags » BSP
Share
WinCE
  • Forum

Browse by Tags

WinCE

Welcome to the WinCE Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
BSP
  • 3530
  • Adeneo
  • AM/DM37x
  • AM3517
  • ARM-A8 WINCE BSP
  • bsp 6.15.00 omap3530 wince6
  • DM3730
  • DSPLINK
  • OMAP
  • OMAP 3530
  • OMAP EVM BSP WinCE
  • omap3530
  • OMAP35x
  • OMAP35xx
  • OMAP35xx EVM
  • OMAP35xx EVM BSP
  • WINCE
  • wince BSP
  • WINCE BSP ARM A8
  • WINCE BSP OMAP3530
  • WINCE OMAP3530 BSP
  • WinCE6
  • WINCE7
  • Windows CE
  • WindowsCE
Related Posts
  • Forum Post: Re: how to suspend the ehci driver

    Jatin Jain Jatin Jain
    Hi, Official support for suspend/resume for OMAP3 WINCE BSP on Mistral EVM is from BSP 6.13 onwards. But EHCI suspend/resume is still an open issue and is being debugged. Basically after suspend the EHCI port fails to wake up. This is not deemed to be a chip issue. Also please know that Beagle board...
    on Mar 9, 2010
  • Forum Post: Re: my application gets slower while using remote tools

    Jatin Jain Jatin Jain
    Hi, I'm not sure which remote tools you are using. But most remote tools work over KITL and that works over the ethernet. Remote tools also have components running on the target board taking up cpu (how much depends on what remote tools you are using). So these factors can affect your real time...
    on Mar 9, 2010
  • Forum Post: Re: my application gets slower while using remote tools

    parsh parsh
    hi Jatin thanks a lot for replying. i am using file viewer specifically.Can there be any way of reduing this delay. regards Parsh
    on Mar 9, 2010
  • Forum Post: USB RNDIS KITL + NK from NAND

    parsh parsh
    hi all i am using Beagleboard and TI's BSP v6.12.03 for NAND booting. However with NAND booting and KITL enabled for USB RNDIS KITL booting stops in between. I have debugged and found that UfnPdd_Init function dies in call to StartUSBClock.Is it the same behaviour on EVM board also where it is unable...
    on Mar 9, 2010
  • Forum Post: Re: USB RNDIS KITL + NK from NAND

    Jatin Jain Jatin Jain
    I'm waiting for confirmation on your question from our third party. In the meantime, is Ethernet KITL an option for you? Jatin
    on Mar 10, 2010
  • Forum Post: Re: Win CE6.0 BSP

    Jatin Jain Jatin Jain
    Vinoth, There is significant effort in WinCE BSP port to a new platform/processor. It will not be possible for us to support a completely new BSP port that you are trying to do. I suggest that you contact your local TI representative to see if your company can get access to early drop of WinCE...
    on Apr 6, 2010
  • Forum Post: When will the BSP6.14 be released?

    Sung-IL Sung-IL
    Hi all, Could you please let me know when will the WinCE BSP6.14 version for OMAP3530 be released? And when will the WinCE BSP for AM3517 be released? Thanks and Best Regards, SI.
    on Apr 20, 2010
  • Forum Post: Re: EVMFlash 2.0 Tool not working in VISTA & WINDOWS 7

    Jatin Jain Jatin Jain
    The EVM flash utility has not been verified with Windows 7 or Vista. Recommend using Windows XP for the first time. For subsequent updates to bootloader, Platform builder can be used to flash.
    on Apr 22, 2010
  • Forum Post: Re: Omap L138 LCD

    Jatin Jain Jatin Jain
    Vinoth, As indicated in an earlier post you will have to wait for the WinCE BSP base port for Omap L138. That will include an example WinCE LIDD driver. Jatin
    on Apr 22, 2010
  • Forum Post: Re: USB RNDIS kitl debug broken in 6.13

    Jatin Jain Jatin Jain
    Yes. bSquare has verified that USB RNDIS KITL works in BSP 6.14. BSP 6.14 will be available for download tomorrow.
    on Apr 29, 2010
  • Forum Post: Re: CE BSP OTG host mode

    Jatin Jain Jatin Jain
    David, I assume that with BSP 6.14 you don't see this issue anymore. (we have had some forum posts movement recently and hence closing out old/open thread). Thanks. Jatin
    on May 7, 2010
  • Forum Post: Re: USB RNDIS sill broken in 6.14

    Jatin Jain Jatin Jain
    David, The changes in both BSP 6.13 and BSP 6.14 were primarily related to power management. The functionality was verified by bSquare on the EVM Rev G. Not sure why this would not work on your custom hardware. (also without a way to reproduce it on the EVM it would be difficult to make progress on...
    on May 11, 2010
  • Forum Post: How to adapt BSP to an OMAP-3530 based board ( a board derived from Beagle Board )?

    arthur14426 arthur14426
    Hello everyone, An OMAP-3530 based board is used in our project. The board (ICETEK-OMAP3530-MINI V3) is get from RealtimeDSP( www.realtimedsp.com.cn ) , which derived from Beagle-Board , and It has more memory( 256M Byte mDDR and 512M Byte Nand Flash ) , and has a VGA-Adapter subboard ( an VGA DAC...
    on May 13, 2010
  • Forum Post: Re: PRM_VOLTCTRL register clearification

    Jatin Jain Jatin Jain
    David, WinCE code is indeed setting the 2 bits contrary to what the TRM says. A bug report has been files for this to be looked at/fixed in a subsequent release. Thanks. Jatin
    on Jun 16, 2010
  • Forum Post: Re: How to compile the VideoCapture source code in WinCE BSP 6.14.00???

    Jatin Jain Jatin Jain
    Hi, Use the instructions in the attached readme.txt file. The readme.txt in the BSP 6.14.00 release is the incorrect version. But do note that there is a dependency on building the video capture source code in the MS shared source tree as is before you can proceed and if that step fails (as specified...
    on Jun 17, 2010
  • Forum Post: Re: Potential bug / typo in prcm_device.h (BSP 6.14)

    Jatin Jain Jatin Jain
    Looks like a bug and a bug report has been opened. The DSS1/DSS2 clk settings seems to be handled in pairs in most places in code and hence maybe no ill-effects of this have been observed. Regardless it should be fixed. Thanks for posting.
    on Jun 25, 2010
  • Forum Post: Re: bsp6.14.00 suspend power measurement

    Jatin Jain Jatin Jain
    Hi, Under the Documentation folder you will see an appnote for Power Management which has measurement numbers. What you observe is expected due to an EHCI driver suspend issue. The document power numbers are without EHCI driver in the build (that is documented in the same section). This will get fixed...
    on Jul 1, 2010
  • Forum Post: Re: reboot the device using "KernelIoControl"

    Jatin Jain Jatin Jain
    Sathish, The BSP version they are using is significantly old (more than 1.5 years I think). Can they download the latest BSP 6.14.00 and try that on the EVM: Using the shell command "reboot". ==> this one uses the IOCTL_HAL_REBOOT. You can run this command if you don't have KITL...
    on Jul 1, 2010
  • Forum Post: Re: back to back uSD card file reads

    Jatin Jain Jatin Jain
    The problem is probably due to the SDHC/SD memory/FATFS subsystem in the bootloader only being designed for one shot use (in the XLDR it loads EBOOTSD.NB0 and then EBOOTSD loads NK.BIN). Changing E BOOT code to load other files from the SD card is not a normal feature of the bootloader and needs...
    on Jul 6, 2010
  • Forum Post: Re: Suspend/resume issue in EHCIPDD, BSP 6.14.01

    Jatin Jain Jatin Jain
    Carsten, Thanks for the detailed analysis/first level fix suggestion. Could you confirm a few things on your setup before your fix. 1. When you see the problem (under the various conditions you mentioned) can you wait for a little while and see if the board recovers (after about 30 seconds). I...
    on Jul 23, 2010
  • Forum Post: Re: GPIO driver implementation bug

    Jatin Jain Jatin Jain
    Thanks. Looks like a valid problem. We will open up a bug report and incorporate it into a future release.
    on Aug 4, 2010
  • Forum Post: Re: Adeneo FTP address ?

    Jatin Jain Jatin Jain
    Okay. The BSP is still not available for general download. But since you have build 9, I would recommend using the same channel for the updated release as well.
    on Aug 5, 2010
  • Forum Post: Re: Adeneo FTP address ?

    Gary Tominovich Gary Tominovich
    The latest version is BSP_WINCE_ARM_A8-1.00.00.11. However, it is only available for limited access via a password-controlled FTP site. You can acquire it from the same location as from where you downloaded the 1.00.00.09 build. If you're not sure of where that is or have forgotten the credentials...
    on Aug 5, 2010
  • Forum Post: Re: Adeneo FTP address ?

    wang jinliang wang jinliang
    Thanks
    on Aug 5, 2010
  • Forum Post: Re: Struggling with USB on OMAP 3530 EVM

    Jatin Jain Jatin Jain
    Dan, The EHCI port should work fine with the BSP 6.14.01.01 release. To narrow down the issue, 1. Did you use these board with a previous version of BSP and was the port working fine? 2. Can you download the prebuilt 6.14.01.01 Demo images from the BSP download page and boot the image (under...
    on Aug 6, 2010
123
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use