• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » WinCE » All Tags » WINCE BSP ARM A8
Share
WinCE
  • Forum

Browse by Tags

WinCE

Welcome to the WinCE Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
WINCE BSP ARM A8
  • 3530
  • AM/DM37x
  • AM3517
  • ARM-A8 WINCE BSP
  • BSP
  • DM3730
  • OMAP
  • OMAP 3530
  • OMAP EVM BSP WinCE
  • omap3530
  • omap3530 wince7
  • OMAP35x
  • OMAP35xx
  • OMAP35xx EVM
  • OMAP35xx EVM BSP
  • WINCE
  • wince BSP
  • WINCE BSP OMAP3530
  • WinCE Compact 7
  • WINCE OMAP3530 BSP
  • WinCE OMAP35x TPS659xx
  • WinCE6
  • WINCE7
  • Windows CE
  • WindowsCE
Related Posts
  • Forum Post: Re: ActiveSync couldn't work on BSP_WINCE_ARM_A8-1.00.00.13.

    Madhvi Madhvi
    Which platform are you trying? OMAP3530 or AM3517? If its OMAP, then you need to use the "do usbFnSet" command (through telnet or command window on LCD) and switch to serial (do usbFnSet serial). If its AM3517, then you need a build with only active sync USB function selected in the catalog...
    on Oct 14, 2010
  • Forum Post: Re: ISR implementation for Timer interrupt on OMAP3530 EVM

    Sho Masuda Sho Masuda
    Hi Jatin, Actually, I don't have any comparison benchmark on other chip, so I cannot be sure this result is not accurate (or is accurate). I just wondered because the IST latency value is much smaller than I thought. According to one of results obtained from internet as shown below, ISR and IST...
    on Oct 18, 2010
  • Forum Post: Re: ISR implementation for Timer interrupt on OMAP3530 EVM

    Sho Masuda Sho Masuda
    Hi Jatin, I succeeded to run ILTiming.exe properly on Compact 7 by modifying some codes related to the timer. In 6.15.00, there are few modifications compared with 6.14.01, but lots of modifications compared with 6.13.00. It seemed quite troublesome to compare and modify all of them, so I just modified...
    on Oct 19, 2010
  • Forum Post: Re: shell bug

    Madhvi Madhvi
    Hi David yes, there is an exception when accessing intwl and outtwl commands due to IOCTL not available to user space processes/modules. In the next release, these commands will be deprecated and removed. One should use the ini2c commands to access the twl regs. The first argument should be 1 (as...
    on Dec 14, 2010
  • Forum Post: Re: Please help me install WinCE demo images on AM3517 eval board

    Madhvi Madhvi
    Hi Reinyn The TI sd card utility is to be used on SD card and not USB stick since USB stick is not a supported boot device in WINCE BSP. Follow instructions in Quick start guide (http://processors.wiki.ti.com/index.php/WinCE-BSP_ARM-A8_Quick_Start_Guide#Standalone_Boot) on how to boot from SD card...
    on Dec 14, 2010
  • Forum Post: Build Error when using WinCE 6.0 R3 WINCE_SDK 01.00.00 for OMAP35x

    Luan Le Luan Le
    Hi, Would you please show me how to have the library file "xamlruntime.lib" created since I got the build error as shown below? Building LINK Pass in C:\WINCE600\PLATFORM\EVM_OMAP3530\SRC\APP\XAMLPERF\ directory. BUILD: [01:0000022306:ERRORE] NMAKE : U1073: don't know how to make...
    on Dec 14, 2010
  • Forum Post: How to set GPIO Debounce time with Unified BSP 1.00?

    Luan Le Luan Le
    Hi, In PddInitializeHardware(VOID) of touchscreen.c BSP6.15.00, the following code are for setting the debounce time of PenIRQ pin: IOCTL_GPIO_SET_DEBOUNCE_TIME_IN debounce; debounce.gpioId = s_TouchDevice.nPenGPIO; debounce.debounceTime = 10; GPIOIoControl(s_TouchDevice.hGPIO...
    on Dec 17, 2010
  • Forum Post: "set BSP_SDRAM_BANK1_ENABLE=0" with WinCE Unified BSP 1.00 causes EVM3530 to hang

    Luan Le Luan Le
    Hi, For my custom board to work, I always have BSP_SDRAM_BANK1_ENABLE set to 0. Since I started using Unified BSP 1.00 , I could no longer be able to download the OS image to my custom board through RNDIS USB, so I went back to the EVM for the baseline. When setting BSP_SDRAM_BANK1_ENABLE = 1,...
    on Dec 18, 2010
  • Forum Post: Re: "set BSP_SDRAM_BANK1_ENABLE=0" with WinCE Unified BSP 1.00 causes EVM3530 to hang

    Madhvi Madhvi
    Luan here are the steps that I followed: 1. Fix init.c to not add CMEM1 region when BANK1 is not enabled 2. Unset BSP_SDRAM_BANK1_ENABLE in EVM_OMAP3530.bat 3. Rebuild BSP (You need to re-build and not just build) 4. Update the XLDR and EBOOT on the device 5. Download NK.bin and boot...
    on Dec 21, 2010
  • Forum Post: Need help with USB RNDIS connection - WinCe Unified BSP and OMAP3530-based board

    Luan Le Luan Le
    Hi everyone, Since switching to the Unified BSP from BSP6.15.00, I am no longer able to have a USB RNDIS connection between Platform Builder and my custom board to download the image. My board does not have the Ethernet port so I am using the OTG USB port on the TPS65930 for the USB RNDIS connection...
    on Dec 24, 2010
  • Forum Post: WINCE_SDK 01.01.00 Release Now Available For Customer Download

    Gary Tominovich Gary Tominovich
    The WinCE 6.0 R3 WINCE_SDK 01.01.00 release is now available for customer download. This is a maintenance update and includes support for the following EVMs/devices: TMDSEVM3530 (OMAP35x) TMDSEVM3517 (AM35x) TMDSEVM3730 (AM/DM37x) To download the release, goto page...
    on Mar 1, 2011
  • Forum Post: How to increase XLDRSD code space on ARM_A8_01_01 BSP?

    Luan Le Luan Le
    Hello, For my custom board to boot, I did some changes in the files xldrnand.bib and xldrtocnand.raw.to increase the size of the NAND XLDR by 4k. In xldrnand.bib, I changed from XLDRNAND 40200000 00008FF8 RAMIMAGE to XLDRNAND 40200000 00009FF8 RAMIMAGE In xldrtocnand.raw, I changed from...
    on Apr 6, 2011
  • Forum Post: Re: USB Problem with an unmodified version of BSP_WINCE_ARM_A8_01_02_00 or BSP_WINCE_ARM_A8_01_01_00_patch_01

    Edward Qing Edward Qing
    Hi,Atul: You can meet the problem in EVM3530,as follow: Running normally, insert a usb memory with many different files, enter usb memory, all the files will be displayed one by one, then press "PWR_ON" button, the system will hang up. In our target board, For example, When reading a...
    on Jun 22, 2011
  • Forum Post: How to turn off these power resources: VINTDIG VINTANA1 VINTANA2 , Baced of BSP_A8_01_02_00 at EVM3730/EVM3530 ?

    Edward Qing Edward Qing
    Hi,All: In order to reduce power consumption, When suspend , Can I turn Off these power resources: VINTDIG VINTANA1 VINTANA2 ? And how to do that ? Thanks! Edward
    on Jun 30, 2011
  • Forum Post: Re: USB Problem with an unmodified version of BSP_WINCE_ARM_A8_01_02_00 or BSP_WINCE_ARM_A8_01_01_00_patch_01

    Edward Qing Edward Qing
    Someone here met same problem? Would you someone give some advices? Thanks ! Edward Qing
    on Jun 30, 2011
  • Forum Post: Windows Embedded Compact Framework 7 - Silverlight compatibility problem

    Zack Zadecki Zack Zadecki
    Hi, I've installed WinCE 7.0 with the A8_02_00_00 TI BSP and using this environment I'd like to test a Silverlight 3 project we have. This project (solution) was created using Expression Blend 4 (with Silverlight 3 option), but it can be successfully open also in Expression Blend 3. After...
    on Jul 1, 2011
  • Forum Post: Adding second NAND memory region/partion from Bootloader?

    Luan Le Luan Le
    Hello, I want to have a separate memory region in NAND to store copies of critical data using the file system. I do not want to store the copies in the same memory region in case that the memory corruption occurs. I am thinking about making the first partition smaller and using the rest of space...
    on Jul 6, 2011
  • Forum Post: DVSDK on DM3730, can't decode h.264 with 720p CODEC

    Jeffrey Hill Jeffrey Hill
    I have a device platform built with the latest releases of the BSP (BSP_WINCE_ARM_A8_01_02_00) and DVSDK (DVSDK_WINCE_01_11_00_03_patch_01), and it is working well. However, when I enable the 720p CODECs and rebuild the image, I can no longer play the h.264-encoded sample Davinci Effect video (or other...
    on Jul 13, 2011
  • Forum Post: CPEN on USB3320 driving USB power

    Zack Zadecki Zack Zadecki
    Hi, We have a custom board with one of two processors: 3530 or 3730. The earlier ones were made with 3530, and the latest ones - with 3730. With both solutions we have the USB3320 chip managing the EHCI USB port. In the latest release we’ve added chips switching (on/off) the power signal to...
    on Aug 2, 2011
  • Forum Post: where to download wince image in nandflash for am3517 EVM?

    token token
    hi, I have start the AM3517EVM from nandflash,but I don't know the adress of the official wince image demo to download, and I don't find any informations in the user guides( WinCE-BSP ARM-A8 User Guide and WinCE-BSP ARM-A8 Quick Start Guide ). could you help me? where's the informations...
    on Aug 15, 2011
  • Forum Post: Inconsistent Resume Power State in DM3730 EVM

    David Stewart David Stewart
    Setup: DM3730 EVM with BSP_WINCE_ARM_A8_01_02_00 There seems to be an inconsistency as to which power state the system returns into upon resuming. When suspending using the power key, devices all go into D4 state. When resuming also using the power, the system resumes to D2. SOMETIMES, but not always...
    on Oct 25, 2011
  • Forum Post: Does WinCE6.0 BSP EMAC driver support operation of 10Base-T on AM3505?

    RY9983 RY9983
    Hello, I am evaluating AM3505 on WindowsCE6.0 with WINCE_SDK 01_01_00_Patch01. Although I would like to operate EMAC via 10Base hub, it have failed on AM3517EVM. (I can access the network via 100Base hub.) - Does WinCE6.0 BSP EMAC driver support operation of 10Base-T on AM35xx? Best regards...
    on Oct 31, 2011
  • Forum Post: Re: Video flicker on WinCE OMAP 3530 with TI DVSDK

    ajit basarur ajit basarur
    Dear Aparna/Madhvi, We are still facing the video flicker issue in latest BSP 01.02.00 and dvsdk_wince_01_11_00_02 package. Can you please let me know if any patch has been released by TI to fix the flicker issue? Regards, Sineesh
    on Nov 21, 2011
  • Forum Post: WEC7 Memory Leakage

    jojo tai jojo tai
    Hi, I use AM3517EVM and WEC7, and found memory loss problems. I use C # to write a small program to reproduce this problem. The program includes twenty Label with a Counter and Timer. In every Time Tick Counter++, and display on the Label. In this way memory is consumed very quickly. ...
    on Dec 19, 2011
  • Forum Post: WinCE 6 busy/unresponsive after copy/paste files

    Luca Cornacchia Luca Cornacchia
    The issue we are dealing with comes up when we try to copy files from objectstore to the same directory into the objectstore itself. The following steps must be performed using explorer UI: 1) create a folder '\test' on objectstore containing 50-60 files of different sizes, from a few...
    on Dec 20, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use