This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPD6S300: / TPD2S300 : USB Type C VBUS protection

Part Number: TPD6S300

What type of lightening or other protection do you recommend on the the VBUS power signals from the USB (3.0/3.1/3.2) Type C connector 

  • Hi Shmuel,

    At this time, we do not have any SuperSpeed short-to-VBUS protection. I don't believe this type of device is available in the semiconductor market (i'm not aware of one as of yet).  Most of our customers care more about the CC protection to VBUS. Some of the legacy cables (Type-C to Type-A), CC is pulled up to VBUS and this can cause potential damage if the cable doesn't have the correct pullup/pulldown resistance. In that case, the TPDxS300 helps protect against this type of situation as well.

    I hope this helps! If this answers your question, PLEASE select  This resolved my issue.

    Best Regards,

    Aramis P. Alvarez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.