This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1E10B06: Spice file for TPD1E10B06

Part Number: TPD1E10B06

I am planning to use TPD1E10B06 in my design, for application of clamping voltage to 8V @ 300uA. Please provide the spice model for analysis using simulation.

1 Reply

  • Hello,
    Spice models are not typically used for ESD diodes as they are for a transient spike. If you would like to see the clamping voltage during an ESD event, looking at the TLP curve is more useful.
    Are you talking about 8V at 300uA DC? The minimum breakdown voltage for the part is 6V at 1mA

    Regards,
    Cameron

    Regards,

    Cameron Phillips
    Applications | ESD & Surge Protection
    c-phillips@ti.com

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.