Hello,
My plan is to replace ESD5304 with TPD4E02B04 in my customer. It is used on the HDMI interface.
Now my problem is the peak power and current of tpd4e02b04 are lower than competitor as belows:
ESD5304: Peak pulse power (tp=8/20us) 82W
Peak pulse Current (tp=8/20us) 5.5A
TPD4E02B04: IEC61000-4-5 Power (tp=8/20us) 17W
IEC61000-4-5 Current (tp=8/20us) 2A
Can you tell me the real meaning of these two parameters ? And give me some advice to persuade my customer to use TPD4E02B04?
The datasheet of ESD5304 is as attached .
Thx.