This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4S214: TPD4S214 DET Pin Issue

Part Number: TPD4S214

Hi.

We are having trouble designing the TPD4S214 and have an inquiry.

The FLT pin and the ADJ pin are floating in the circuit, and the EN pin is controlled by the controller.

The problem is that the signal of the DET Pin is set to Low and it can not be changed.

The DET pin is LOW when both the USB connection and the connection are disabled.

The DET pin has a circuit connection to the controller.

I would like to know if the FL pin and ADJ pin are floating and the DET pin can not be changed.

And one more question. Is it possible to check if the TPD4S214 Spec has an Automotive product that supports Host and OTG at the same time?

Thanks,

Best regards, 

Tyler