Using this device for something slightly different than ESD protection. Using it to clamp a pulse that is a bit longer than the profiles it is defined for:
E.g. if hit with 150mA for 20ms, is that ok?
The spec does not help answer if this is possible. Max ratings indicate 3A and 45W but for the 8/20us pulse. If that is the max energy (possibly about 0.4mJ), then it would not be able to handle the example above. Is there a spec for how much energy it can absorb? In Joules? How do we get a handle on this?
Thanks..