Other Parts Discussed in Thread: TPS65981EVM
Hi,
For a USB type-C UFP design, Where do we need to have RPD_Gx pins shorted to CCx pins for dead battery condition?
1. Is it near TPD8S300 side only?
2. Is it near TPS65986 side only?
3. Is it near both TPD8S300 side & TPS65986 side?
In our design by default the RPD_Gx pins shorted to CCx pin only near TPD8S300. It power ON the board, but it does not enumerates the USB device . However if I connect the RPD_Gx pins to CCx pin near TPS65986, it is working. So my doubt here is, in dead battery condition the OVP FET inside TPD8S300 isolates these RD resistors in the CC/PD controller when no power. Then how the RD resistor near TPS65986 will be seen by USB source to detect dead battery condition.
Attached the Schematic for reference. Please help clarifying this.
Thanks
Pandiyarajan