This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

USB TYPE C VBUS Protection

What type of protection on the VBUS do you recommend for the USB (3.0/3.1/3.2) Type C connector ? 

In previous USB 2.0 Designs we have used a Littlefuse PGB1010603 PULSE-GUARD® ESD Suppressors

We are using both the TI TPD6S300 and TI TPD2S300 to protect the other USB Type C signals ! 

  • Hi Shmuel,

    I believe the question you're asking was answered in a previous thread, which can be found here: https://e2e.ti.com/support/interface/circuit-protection/f/389/t/650941

    I recommend placing high-speed ESD diodes (TPD1E5B04DPYR) on each USB3.1 channels. Feel free to look at one of our PD controller EVM schematic, such as the TPS65981-EVM. Page 23 of the user's guide shows the connection of these ESD diodes on the Type-C connector (look below):

    It's also recommended to place a Schottky diode and a 0.1uF cap on each VBUS channel.

    Lastly, I don't beleive you need both the TPD6s300 and TPD2s300. You would need just one of these protection devices per Type-C port.

    TPD2s300: CCx protection

    TPD6s300: CCx, SBUx, and one USB2.0 channel protection

    TPD8s300: CCx, SBUx, and both USB2.0 channel protection

    If this answers your question, PLEASE select  This resolved my issue 

    Best Regards,

    Aramis P. Alvarez

  • In reply to Aramis P. Alvarez:

    Dear Aramis,

    Thank you so much for this reply, it has helped me a lot in getting a better understanding of the circuit protection requirements. I am now looking at the schematic of the TPS65981-EVM and seeing there is a lot more protection on that board that what I have planned ! 

    Firstly we are NOT going to be using \ designing USB PD. To get enough power we have planned to use 2 Type C connectors one for Communication and power and the 2nd connector solely for additional power. This explains why we are using both the  the TPD6s300 and TPD2s300

    1. I see that there are Schottky diodes D4-D10, & D12 on the Tx\Rx lines ! For my non-PD design is this required \ recommended ?

    2. In the HD3SS3220 data sheet they mention using "the TI TPD4EUSB30 can be combined with the TI TPD2EUSB30 to provide flow-through ESD protection for both USB2 and USB3 differential signals". (This probably answers my above question ?) WHen I looked at these data sheets they are for USB 3.0 as expected. Would it be better to use a similar device but that give protection for USB 3.1 since we might go to that in the future ? Thus we will only need to stock 1 device if it is compatible with both 3.0 & 3.1 ?! What do you recommend ? Would, lets say TPD4E02B04-Q1 be a better choice ?

    3. We will be using the FTDI FT601 chip to do the interfacing to the USB 3.0 bus. In our previous USB 2.0 design FTDI recommended also PulseGuard ESD Suppressors - PGB1010603 on the USB 2.0 DP/DM signals as well as 10pF Caps to GND. When I asked them about this requirement for this design using the FT601 they claimed that it was necessary as a different PHY is being used. When I looked at the data sheet for the FT601 ESD and Latch-up Specifications :-

    Human Body Mode (HBM)  - JEDEC EIA/JESD22- A114-B, Class 2 - ±2kV 

    Machine mode (MM) - JEDEC EIA/JESD22- A115-A, Class B - ±200V

    Charged Device Mode (CDM) - JEDEC EIA/ JESD22-C101- D, Class-III - ±500V

    Latch-up JESD78, Trigger Class-II - ±200mA

    In your opinion is this enough ? In the TPD4E02B04-Q1 data sheet they recommend on the USB 2.0 lines to use TPD4E05U06-Q1 ? What do you think ?

  • In reply to Shmuel Davis:

    Hi Shmuel,

    I'm always happy to help. The ESD diodes are recommended on the USB 3.1 (USB 3.0, 3.1, and 3.2 are all the same channels and pins on the type-c connector) channels. This will protect these pins from any ESD events. The reason I showed the TPS65981-EVM was to show our protection on the Type-C connector (you can disregard the PD controller design for your application).

    For the TPD4/2EUUSB30 device, could you please re-post your question with that part number in the subject heading, so that this question is routed to the appropriate forum and expert engineers? Thanks in advance :-)

    Best Regards,

    Aramis P. Alvarez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.